Check the data sheet of your device for more information. ... For 2 Mbps PHY, it is a few tenths dB more. ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 ...
// Bluetooth LE//Version 2.13 // ... Bluetooth SIG defines a HID profile that specifies how a device can support HID services over the Bluetooth LE protocol stack using the Generic Attribute ...
This lab will set up a Bluetooth server to send the analog data to a Bluetooth client. ... _mv(); // Convert endianess volt_buf[0] = (data_mV >> 8) & 0x00FF; volt_buf[1] = data_mV & 0x00FF;
// Bluetooth LE//Version 2.13 // ... Starting in Bluetooth 5, it is possible to offload the advertising data payload onto one of the data channels. ... Observe the logs on the terminals.
Data is handled transparently, meaning that the transmitted values can be either ASCII strings or binary ... a new SoC - Empty application project with Bluetooth SDK version 2.12 or newer.
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg12/group-dbg