Silicon Labs
gecko-platform/latest/emlib/api/efm32gg12/struct-a-c-m-p-v-a-config-type-def
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
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg12/struct-a-c-m-p-v-a-config-type-def in 0.28 seconds
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a connection is established via J-Link. ... sl_iostream_instance_rtt_info
ProductMicrocontrollers Resource TypeSoftware API documentation
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
Configuration Options The API Flow Control Support ... A UART driver instance handle data structure. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollers Resource TypeSoftware API documentation
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A non periodic timer is considered not running during its callback.
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
... -platform/latest/driver/api/group-uartdrv https://docs.silabs.com/gecko-platform/latest/driver/api/group-ustimer Gecko Platform – Service ... Platform Services Detail Device Initialization
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
    Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg12/struct-a-c-m-p-v-a-config-type-def