Configuration Options The API Flow Control Support ... A UART driver instance handle data structure. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... A 64-bits tick counter is accessible through the ... All API functions can be called from within interrupt handlers. ... void N/A Returns
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32hg/struct-l-e-u-a-r-t-init-type-def