// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A pointer to this function is passed to sl_sleeptimer_start_timer().
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a ... sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
The ZG28 is an ideal platform for Z-Wave applications that require more Flash, RAM and ... names in our industry share and discover the latest trends and technologies that are making our lives ...
ProductWirelessResource TypeProduct Category Page
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32tg11/struct-o-p-a-m-p-init-type-def