Silicon Labs
gecko-platform/latest/emlib/api/efm32xg12/hardware-board/api/group-board-init
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
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/hardware-board/api/group-board-init in 0.27 seconds
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
... group-board-control https://docs.silabs.com/gecko-platform/latest/hardware-board/api/group-board-init https://docs.silabs.com/gecko-platform/ ... Platform Services Detail Device Initialization
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Hardware block inside the SE used for generating random numbers.
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables ... Function Documentation ◆ sl_iostream_rtt_init() sl_status_t sl_iostream_rtt_init ... ) RTT Stream init. Returns
ProductMicrocontrollers Resource TypeSoftware API documentation
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
Configuration Options The API Flow Control Support ... in the init struct. GPIO Hardware Flow Control To support hardware flow control on devices that don't have UART CTS/RTS hardware ...
ProductMicrocontrollers Resource TypeSoftware API documentation
    Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/hardware-board/api/group-board-init