Login ... // Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible.
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Configuration Options The API Flow Control Support ... This section contains brief descriptions of the functions in the API. ... The application code must include uartdrv.h header file.
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/middleware/api/struct-b-m-p-header