Error Codes#
Macros#
#define
ECODE_EMDRV_SPIDRV_OK (ECODE_OK)
A successful return value.
#define
ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE (ECODE_EMDRV_SPIDRV_BASE | 0x00000001)
An illegal SPI handle.
#define
ECODE_EMDRV_SPIDRV_PARAM_ERROR (ECODE_EMDRV_SPIDRV_BASE | 0x00000002)
An illegal input parameter.
#define
ECODE_EMDRV_SPIDRV_BUSY (ECODE_EMDRV_SPIDRV_BASE | 0x00000003)
The SPI port is busy.
#define
ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR (ECODE_EMDRV_SPIDRV_BASE | 0x00000004)
Unable to allocate timeout timer.
#define
ECODE_EMDRV_SPIDRV_TIMEOUT (ECODE_EMDRV_SPIDRV_BASE | 0x00000005)
An SPI transfer timeout.
#define
ECODE_EMDRV_SPIDRV_IDLE (ECODE_EMDRV_SPIDRV_BASE | 0x00000006)
No SPI transfer in progress.
#define
ECODE_EMDRV_SPIDRV_ABORTED (ECODE_EMDRV_SPIDRV_BASE | 0x00000007)
An SPI transfer has been aborted.
#define
ECODE_EMDRV_SPIDRV_MODE_ERROR (ECODE_EMDRV_SPIDRV_BASE | 0x00000008)
SPI master used slave API or vica versa.
#define
ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR (ECODE_EMDRV_SPIDRV_BASE | 0x00000009)
Unable to allocate DMA channels.
#define
ECODE_EMDRV_SPIDRV_ALREADY_INITIALIZED (ECODE_EMDRV_SPIDRV_BASE | 0x0000000A)
The SPI handle is already initialized.
Macro Definition Documentation#
ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLE#
#define ECODE_EMDRV_SPIDRV_ILLEGAL_HANDLEValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000001)
An illegal SPI handle.
ECODE_EMDRV_SPIDRV_PARAM_ERROR#
#define ECODE_EMDRV_SPIDRV_PARAM_ERRORValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000002)
An illegal input parameter.
ECODE_EMDRV_SPIDRV_BUSY#
#define ECODE_EMDRV_SPIDRV_BUSYValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000003)
The SPI port is busy.
ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERROR#
#define ECODE_EMDRV_SPIDRV_TIMER_ALLOC_ERRORValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000004)
Unable to allocate timeout timer.
ECODE_EMDRV_SPIDRV_TIMEOUT#
#define ECODE_EMDRV_SPIDRV_TIMEOUTValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000005)
An SPI transfer timeout.
ECODE_EMDRV_SPIDRV_IDLE#
#define ECODE_EMDRV_SPIDRV_IDLEValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000006)
No SPI transfer in progress.
ECODE_EMDRV_SPIDRV_ABORTED#
#define ECODE_EMDRV_SPIDRV_ABORTEDValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000007)
An SPI transfer has been aborted.
ECODE_EMDRV_SPIDRV_MODE_ERROR#
#define ECODE_EMDRV_SPIDRV_MODE_ERRORValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000008)
SPI master used slave API or vica versa.
ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERROR#
#define ECODE_EMDRV_SPIDRV_DMA_ALLOC_ERRORValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x00000009)
Unable to allocate DMA channels.
ECODE_EMDRV_SPIDRV_ALREADY_INITIALIZED#
#define ECODE_EMDRV_SPIDRV_ALREADY_INITIALIZEDValue:
(ECODE_EMDRV_SPIDRV_BASE | 0x0000000A)
The SPI handle is already initialized.