LESENSE - Low Energy Sensor#

Low Energy Sensor (LESENSE) Peripheral API.

This module contains functions to control the LESENSE peripheral of Silicon Labs 32-bit MCUs and SoCs. LESENSE is a low-energy sensor interface capable of autonomously collecting and processing data from multiple sensors even when in EM2.

Modules#

LESENSE_CoreCtrlDesc_TypeDef

LESENSE_TimeCtrlDesc_TypeDef

LESENSE_PerCtrlDesc_TypeDef

LESENSE_DecCtrlDesc_TypeDef

LESENSE_Init_TypeDef

LESENSE_ChDesc_TypeDef

LESENSE_ChAll_TypeDef

LESENSE_AltExDesc_TypeDef

LESENSE_ConfAltEx_TypeDef

LESENSE_DecStCond_TypeDef

LESENSE_DecStAll_TypeDef

Enumerations#

enum
lesenseClkDiv_1 = 0
lesenseClkDiv_2 = 1
lesenseClkDiv_4 = 2
lesenseClkDiv_8 = 3
lesenseClkDiv_16 = 4
lesenseClkDiv_32 = 5
lesenseClkDiv_64 = 6
lesenseClkDiv_128 = 7
}

Clock divisors for controlling the prescaling factor of the period counter.

enum
lesenseScanStartPeriodic = LESENSE_CFG_SCANMODE_PERIODIC
lesenseScanStartOneShot = LESENSE_CFG_SCANMODE_ONESHOT
lesenseScanStartPRS = LESENSE_CFG_SCANMODE_PRS
}

Scan modes.

enum
lesensePRSCh0 = 0
lesensePRSCh1 = 1
lesensePRSCh2 = 2
lesensePRSCh3 = 3
lesensePRSCh4 = 4
lesensePRSCh5 = 5
lesensePRSCh6 = 6
lesensePRSCh7 = 7
lesensePRSCh8 = 8
lesensePRSCh9 = 9
lesensePRSCh10 = 10
lesensePRSCh11 = 11
}

PRS sources.

enum
lesenseDMAWakeUpDisable = LESENSE_CFG_DMAWU_DISABLE
lesenseDMAWakeUpEnable = LESENSE_CFG_DMAWU_ENABLE
}

Modes of operation for DMA wakeup from EM2.

enum
lesenseScanConfDirMap = LESENSE_CFG_SCANCONF_DIRMAP
lesenseScanConfInvMap = LESENSE_CFG_SCANCONF_INVMAP
lesenseScanConfToggle = LESENSE_CFG_SCANCONF_TOGGLE
lesenseScanConfDecDef = LESENSE_CFG_SCANCONF_DECDEF
}

Scan configuration.

enum
lesenseDACIfData = _LESENSE_PERCTRL_DACCH0DATA_DACDATA
lesenseThres = _LESENSE_PERCTRL_DACCH0DATA_THRES
}

DAC CHx data control configuration.

enum
lesenseACMPModeMux = _LESENSE_PERCTRL_ACMP0MODE_MUX
lesenseACMPModeMuxThres = _LESENSE_PERCTRL_ACMP0MODE_MUXTHRES
}

ACMPx control configuration.

enum
lesenseSampleModeCounter = LESENSE_CH_INTERACT_SAMPLE_ACMPCOUNT
lesenseSampleModeACMP = LESENSE_CH_INTERACT_SAMPLE_ACMP
lesenseSampleModeADC = LESENSE_CH_INTERACT_SAMPLE_ADC
lesenseSampleModeADCDiff = LESENSE_CH_INTERACT_SAMPLE_ADCDIFF
}

Decoder input source configuration.

enum
lesenseSetIntNone = LESENSE_CH_INTERACT_SETIF_NONE
lesenseSetIntLevel = LESENSE_CH_INTERACT_SETIF_LEVEL
lesenseSetIntPosEdge = LESENSE_CH_INTERACT_SETIF_POSEDGE
lesenseSetIntNegEdge = LESENSE_CH_INTERACT_SETIF_NEGEDGE
lesenseSetIntBothEdges = LESENSE_CH_INTERACT_SETIF_BOTHEDGES
}

Interrupt generation setup for CHx interrupt flag.

enum
lesenseChPinExDis = LESENSE_CH_INTERACT_EXMODE_DISABLE
lesenseChPinExHigh = LESENSE_CH_INTERACT_EXMODE_HIGH
lesenseChPinExLow = LESENSE_CH_INTERACT_EXMODE_LOW
lesenseChPinExDACOut = LESENSE_CH_INTERACT_EXMODE_DACOUT
}

Channel pin mode for the excitation phase of the scan sequence.

enum
lesenseChPinIdleDis = _LESENSE_IDLECONF_CHIDLE0_DISABLE
lesenseChPinIdleHigh = _LESENSE_IDLECONF_CHIDLE0_HIGH
lesenseChPinIdleLow = _LESENSE_IDLECONF_CHIDLE0_LOW
lesenseChPinIdleDACC = _LESENSE_IDLECONF_CHIDLE0_DAC
}

Channel pin mode for the idle phase of scan sequence.

enum
lesenseClkLF = _LESENSE_CH_INTERACT_EXCLK_LFACLK
lesenseClkHF = _LESENSE_CH_INTERACT_EXCLK_AUXHFRCO
}

Clock used for excitation and sample delay timing.

enum
lesenseCompModeLess = LESENSE_CH_EVALCFG_COMP_LESS
lesenseCompModeGreaterOrEq = LESENSE_CH_EVALCFG_COMP_GE
}

Compare modes for counter comparison.

enum
lesenseStoreSampleDisable = _LESENSE_CH_EVALCFG_STRSAMPLE_DISABLE
lesenseStoreSampleData = _LESENSE_CH_EVALCFG_STRSAMPLE_DATA
lesenseStoreSampleDataSrc = _LESENSE_CH_EVALCFG_STRSAMPLE_DATASRC
}

Mode of Storing of Sensor Sample in Result Buffer.

enum
lesenseEvalModeThreshold = _LESENSE_CH_EVALCFG_MODE_THRES
lesenseEvalModeSlidingWindow = _LESENSE_CH_EVALCFG_MODE_SLIDINGWIN
lesenseEvalModeStepDetection = _LESENSE_CH_EVALCFG_MODE_STEPDET
}

Sensor evaluation modes.

enum
lesenseTransActNone = LESENSE_ST_ARC_PRSACT_NONE
lesenseTransActPRS0 = LESENSE_ST_ARC_PRSACT_PRS0
lesenseTransActPRS1 = LESENSE_ST_ARC_PRSACT_PRS1
lesenseTransActPRS01 = LESENSE_ST_ARC_PRSACT_PRS01
lesenseTransActPRS2 = LESENSE_ST_ARC_PRSACT_PRS2
lesenseTransActPRS02 = LESENSE_ST_ARC_PRSACT_PRS02
lesenseTransActPRS12 = LESENSE_ST_ARC_PRSACT_PRS12
lesenseTransActPRS012 = LESENSE_ST_ARC_PRSACT_PRS012
lesenseTransActUp = LESENSE_ST_ARC_PRSACT_UP
lesenseTransActDown = LESENSE_ST_ARC_PRSACT_DOWN
lesenseTransActUpAndPRS2 = LESENSE_ST_ARC_PRSACT_UPANDPRS2
lesenseTransActDownAndPRS2 = LESENSE_ST_ARC_PRSACT_DOWNANDPRS2
}

Transition action modes.

Typedefs#

Decoder state x configuration structure.

Functions#

void
LESENSE_Init(const LESENSE_Init_TypeDef *init, bool reqReset)

Initialize the LESENSE module.

uint32_t
LESENSE_ScanFreqSet(uint32_t refFreq, uint32_t scanFreq)

Set the scan frequency for periodic scanning.

void
LESENSE_ScanModeSet(LESENSE_ScanMode_TypeDef scanMode, bool start)

Set scan mode of the LESENSE channels.

void
LESENSE_StartDelaySet(uint8_t startDelay)

Set the start delay of the sensor interaction on each channel.

void
LESENSE_ClkDivSet(LESENSE_ChClk_TypeDef clk, LESENSE_ClkPresc_TypeDef clkDiv)

Set the clock division for LESENSE timers.

void
LESENSE_ChannelAllConfig(const LESENSE_ChAll_TypeDef *confChAll)

Configure all (16) LESENSE sensor channels.

void
LESENSE_ChannelConfig(const LESENSE_ChDesc_TypeDef *confCh, uint32_t chIdx)

Configure a single LESENSE sensor channel.

void
LESENSE_AltExConfig(const LESENSE_ConfAltEx_TypeDef *confAltEx)

Configure the LESENSE alternate excitation modes.

void
LESENSE_ChannelEnable(uint8_t chIdx, bool enaScanCh, bool enaPin)

Enable/disable LESENSE scan channel and the pin assigned to it.

void
LESENSE_ChannelEnableMask(uint16_t chMask, uint16_t pinMask)

Enable/disable LESENSE scan channel and the pin assigned to it.

void
LESENSE_ChannelTimingSet(uint8_t chIdx, uint8_t exTime, uint8_t sampleDelay, uint16_t measDelay)

Set LESENSE channel timing parameters.

void
LESENSE_ChannelThresSet(uint8_t chIdx, uint16_t acmpThres, uint16_t cntThres)

Set LESENSE channel threshold parameters.

void
LESENSE_ChannelSlidingWindow(uint8_t chIdx, uint32_t windowSize, uint32_t initValue)

Configure a Sliding Window evaluation mode for a specific channel.

void
LESENSE_ChannelStepDetection(uint8_t chIdx, uint32_t stepSize, uint32_t initValue)

Configure the step detection evaluation mode for a specific channel.

void
LESENSE_WindowSizeSet(uint32_t windowSize)

Set the window size for all LESENSE channels.

void
LESENSE_StepSizeSet(uint32_t stepSize)

Set the step size for all LESENSE channels.

void
LESENSE_DecoderStateAllConfig(const LESENSE_DecStAll_TypeDef *confDecStAll)

Configure all LESENSE decoder states.

void
LESENSE_DecoderStateConfig(const LESENSE_DecStDesc_TypeDef *confDecSt, uint32_t decSt)

Configure a single LESENSE decoder state.

uint32_t

Get the current state of the LESENSE decoder.

void
LESENSE_DecoderPrsOut(bool enable, uint32_t decMask, uint32_t decVal)

Enable or disable the PRS output from the LESENSE decoder.

void

Start scanning sensors.

void

Stop scanning sensors.

void

Start the LESENSE decoder.

void

Clear the result buffer.

void

Reset the LESENSE module.

void

Stop LESENSE decoder.

uint32_t

Get the current status of LESENSE.

void
LESENSE_StatusWait(uint32_t flag)

Wait until status of LESENSE is equal to what was requested.

uint32_t

Get the currently active channel index.

uint32_t

Get the latest scan comparison result (1 bit / channel).

uint32_t

Get the oldest unread data from the result buffer.

uint32_t

Get the current state of the LESENSE sensor.

void
LESENSE_IntClear(uint32_t flags)

Clear one or more pending LESENSE interrupts.

void
LESENSE_IntEnable(uint32_t flags)

Enable one or more LESENSE interrupts.

void
LESENSE_IntDisable(uint32_t flags)

Disable one or more LESENSE interrupts.

void
LESENSE_IntSet(uint32_t flags)

Set one or more pending LESENSE interrupts from SW.

uint32_t

Get pending LESENSE interrupt flags.

uint32_t

Get enabled and pending LESENSE interrupt flags.

Macros#

#define
LESENSE_NUM_DECODER_STATES (_LESENSE_DECSTATE_DECSTATE_MASK + 1)

Number of decoder states supported by current device.

#define
LESENSE_NUM_ARCS (LESENSE_NUM_DECODER_STATES << 1)

Number of ARCs supported by current device.

#define

Number of LESENSE channels.

#define

Default configuration for LESENSE_CtrlDesc_TypeDef structure.

#define

Default configuration for LESENSE_TimeCtrlDesc_TypeDef structure.

#define

Default configuration for LESENSE_PerCtrl_TypeDef structure.

#define

Default configuration for LESENSE_PerCtrl_TypeDef structure.

#define

Default configuration for LESENSE_Init_TypeDef structure.

#define

Default configuration for the scan channel.

#define

Default configuration for all the sensor channels.

#define

Default configuration for the alternate excitation channel.

#define

Default configuration for all the alternate excitation channels.

#define

Default configuration for the decoder state condition.

#define

Default configuration for all decoder states.

Enumeration Documentation#

LESENSE_ClkPresc_TypeDef#

LESENSE_ClkPresc_TypeDef

Clock divisors for controlling the prescaling factor of the period counter.

Note: These enumeration values are used for different clock division related configuration parameters (hfPresc, lfPresc, pcPresc).

Enumerator
lesenseClkDiv_1

Divide clock by 1.

lesenseClkDiv_2

Divide clock by 2.

lesenseClkDiv_4

Divide clock by 4.

lesenseClkDiv_8

Divide clock by 8.

lesenseClkDiv_16

Divide clock by 16.

lesenseClkDiv_32

Divide clock by 32.

lesenseClkDiv_64

Divide clock by 64.

lesenseClkDiv_128

Divide clock by 128.


LESENSE_ScanMode_TypeDef#

LESENSE_ScanMode_TypeDef

Scan modes.

Enumerator
lesenseScanStartPeriodic

New scan is started each time the period counter overflows.

lesenseScanStartOneShot

Single scan is performed when LESENSE_ScanStart() is called.

lesenseScanStartPRS

New scan is triggered by pulse on PRS channel.


LESENSE_PRSSel_TypeDef#

LESENSE_PRSSel_TypeDef

PRS sources.

Note: These enumeration values are being used for different PRS related configuration parameters.

Enumerator
lesensePRSCh0

PRS channel 0.

lesensePRSCh1

PRS channel 1.

lesensePRSCh2

PRS channel 2.

lesensePRSCh3

PRS channel 3.

lesensePRSCh4

PRS channel 4.

lesensePRSCh5

PRS channel 5.

lesensePRSCh6

PRS channel 6.

lesensePRSCh7

PRS channel 7.

lesensePRSCh8

PRS channel 8.

lesensePRSCh9

PRS channel 9.

lesensePRSCh10

PRS channel 10.

lesensePRSCh11

PRS channel 11.


LESENSE_DMAWakeUp_TypeDef#

LESENSE_DMAWakeUp_TypeDef

Modes of operation for DMA wakeup from EM2.

Enumerator
lesenseDMAWakeUpDisable

No DMA wakeup from EM2.

lesenseDMAWakeUpEnable

DMA wakeup from EM2.


LESENSE_ScanConfSel_TypeDef#

LESENSE_ScanConfSel_TypeDef

Scan configuration.

Enumerator
lesenseScanConfDirMap

Channel configuration registers (CHx_CONF) used are directly mapped to the channel number.

lesenseScanConfInvMap

Channel configuration registers used are CHx+8_CONF for channels 0-7 and CHx-8_CONF for channels 8-15.

lesenseScanConfToggle

Channel configuration registers used toggles between CHX_SCANCONF and CHX+8_SCANCONF when channel x triggers.

lesenseScanConfDecDef

Decoder state defines the channel configuration register (CHx_CONF) to be used.


LESENSE_ControlDACData_TypeDef#

LESENSE_ControlDACData_TypeDef

DAC CHx data control configuration.

Enumerator
lesenseDACIfData

DAC channel x data is defined by the DAC_CHxDATA register.

lesenseThres

DAC channel x data is defined by the THRES in LESENSE_CHx_INTERACT.


LESENSE_ControlACMP_TypeDef#

LESENSE_ControlACMP_TypeDef

ACMPx control configuration.

Enumerator
lesenseACMPModeMux

LESENSE does not control ACMPx.

lesenseACMPModeMuxThres

LESENSE controls input mux of and threshold value of ACMPx.


LESENSE_ChSampleMode_TypeDef#

LESENSE_ChSampleMode_TypeDef

Decoder input source configuration.

Ocelot only provides SENSORSTATE as input for the decoder. Compare source selection for sensor sampling.

Enumerator
lesenseSampleModeCounter

Counter output will be used in comparison.

lesenseSampleModeACMP

ACMP output will be used in comparison.

lesenseSampleModeADC

ADC output will be used in comparison.

lesenseSampleModeADCDiff

Differential ADC output will be used in comparison.


LESENSE_ChIntMode_TypeDef#

LESENSE_ChIntMode_TypeDef

Interrupt generation setup for CHx interrupt flag.

Enumerator
lesenseSetIntNone

No interrupt is generated.

lesenseSetIntLevel

Set interrupt flag if the sensor triggers.

lesenseSetIntPosEdge

Set interrupt flag on positive edge of the sensor state.

lesenseSetIntNegEdge

Set interrupt flag on negative edge of the sensor state.

lesenseSetIntBothEdges

Set interrupt flag on both edges of the sensor state.


LESENSE_ChPinExMode_TypeDef#

LESENSE_ChPinExMode_TypeDef

Channel pin mode for the excitation phase of the scan sequence.

Enumerator
lesenseChPinExDis

Channel pin is disabled.

lesenseChPinExHigh

Channel pin is configured as push-pull, driven HIGH.

lesenseChPinExLow

Channel pin is configured as push-pull, driven LOW.

lesenseChPinExDACOut

DAC output (only available on channel 0, 1, 2, 3, 12, 13, 14 and 15)


LESENSE_ChPinIdleMode_TypeDef#

LESENSE_ChPinIdleMode_TypeDef

Channel pin mode for the idle phase of scan sequence.

Enumerator
lesenseChPinIdleDis

Channel pin is disabled in idle phase.

lesenseChPinIdleHigh

Channel pin is configured as push-pull, driven HIGH in idle phase.

lesenseChPinIdleLow

Channel pin is configured as push-pull, driven LOW in idle phase.

lesenseChPinIdleDACC

Channel pin is connected to DAC output in idle phase.


LESENSE_ChClk_TypeDef#

LESENSE_ChClk_TypeDef

Clock used for excitation and sample delay timing.

Enumerator
lesenseClkLF

LFACLK (LF clock) is used.

lesenseClkHF

AUXHFRCO (HF clock) is used.


LESENSE_ChCompMode_TypeDef#

LESENSE_ChCompMode_TypeDef

Compare modes for counter comparison.

Enumerator
lesenseCompModeLess

Comparison evaluates to 1 if sensor data is less than the counter threshold, or if ACMP output is 0.

lesenseCompModeGreaterOrEq

Comparison evaluates to 1 if sensor data is greater than, or equal to the counter threshold, or if the ACMP output is 1.


LESENSE_StoreSample_TypeDef#

LESENSE_StoreSample_TypeDef

Mode of Storing of Sensor Sample in Result Buffer.

Enumerator
lesenseStoreSampleDisable

Nothing will be stored in the result buffer.

lesenseStoreSampleData

The sensor sample data will be stored in the result buffer.

lesenseStoreSampleDataSrc

The data source (i.e.


LESENSE_ChEvalMode_TypeDef#

LESENSE_ChEvalMode_TypeDef

Sensor evaluation modes.

Enumerator
lesenseEvalModeThreshold

Threshold comparison evaluation mode.

lesenseEvalModeSlidingWindow

Sliding window evaluation mode.

lesenseEvalModeStepDetection

Step detection evaluation mode.


LESENSE_StTransAct_TypeDef#

LESENSE_StTransAct_TypeDef

Transition action modes.

Enumerator
lesenseTransActNone

No PRS pulses generated (if PRSCOUNT == 0).

lesenseTransActPRS0

Generate pulse on LESPRS0 (if PRSCOUNT == 0).

lesenseTransActPRS1

Generate pulse on LESPRS1 (if PRSCOUNT == 0).

lesenseTransActPRS01

Generate pulse on LESPRS0 and LESPRS1 (if PRSCOUNT == 0).

lesenseTransActPRS2

Generate pulse on LESPRS2 (for both PRSCOUNT == 0 and PRSCOUNT == 1).

lesenseTransActPRS02

Generate pulse on LESPRS0 and LESPRS2 (if PRSCOUNT == 0).

lesenseTransActPRS12

Generate pulse on LESPRS1 and LESPRS2 (if PRSCOUNT == 0).

lesenseTransActPRS012

Generate pulse on LESPRS0, LESPRS1 and LESPRS2 (if PRSCOUNT == 0).

lesenseTransActUp

Count up (if PRSCOUNT == 1).

lesenseTransActDown

Count down (if PRSCOUNT == 1).

lesenseTransActUpAndPRS2

Count up and generate pulse on LESPRS2 (if PRSCOUNT == 1).

lesenseTransActDownAndPRS2

Count down and generate pulse on LESPRS2 (if PRSCOUNT == 1).


Typedef Documentation#

LESENSE_DecStDesc_TypeDef#

typedef LESENSE_DecStCond_TypeDef LESENSE_DecStDesc_TypeDef

Decoder state x configuration structure.


Function Documentation#

LESENSE_Init#

void LESENSE_Init (const LESENSE_Init_TypeDef * init, bool reqReset)

Initialize the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_Init_TypeDef *[in]init

The LESENSE initialization structure.

bool[in]reqReset

Request to call LESENSE_Reset() first to initialize all LESENSE registers with default values.

This function configures the main parameters of the LESENSE interface. See the initialization parameter type definition (LESENSE_Init_TypeDef) for more details.

Note

  • LESENSE_Init() is designed to initialize LESENSE once in an operation cycle. Be aware of the effects of reconfiguration if using this function from multiple sources in your code. This function has not been designed to be re-entrant. Requesting reset by setting reqReset to true is required in each reset or power-on cycle to configure the default values of the RAM mapped LESENSE registers. Notice that GPIO pins used by the LESENSE module must be properly configured by the user explicitly for the LESENSE to work as intended. (When configuring pins, one should remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)


LESENSE_ScanFreqSet#

uint32_t LESENSE_ScanFreqSet (uint32_t refFreq, uint32_t scanFreq)

Set the scan frequency for periodic scanning.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]refFreq

Select reference LFACLK clock frequency in Hz. If set to 0, the current clock frequency is being used as a reference.

uint32_t[in]scanFreq

Set the desired scan frequency in Hz.

This function only applies to LESENSE if a period counter is used as a trigger for scan start. The calculation is based on the following formula: Fscan = LFACLKles / ((1+PCTOP)*2^PCPRESC)

Note

  • Note that the calculation does not necessarily result in the requested scan frequency due to integer division. Check the return value for the resulted scan frequency.

Returns

  • Frequency in Hz calculated and set by this function. Users can use this to compare the requested and set values.


LESENSE_ScanModeSet#

void LESENSE_ScanModeSet (LESENSE_ScanMode_TypeDef scanMode, bool start)

Set scan mode of the LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
LESENSE_ScanMode_TypeDef[in]scanMode

Select the location to map LESENSE alternate excitation channels.

  • lesenseScanStartPeriodic - A new scan is started each time the period counter overflows.

  • lesenseScanStartOneShot - A single scan is performed when LESENSE_ScanStart() is called.

  • lesenseScanStartPRS - A new scan is triggered by pulse on the PRS channel.

bool[in]start

If true, LESENSE_ScanStart() is immediately issued after configuration.

This function configures how the scan start is triggered. It can be used for re-configuring the scan mode while running the application but it is also used by LESENSE_Init() for initialization.

Note

  • Users can configure the scan mode by LESENSE_Init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Be aware of the effects of the non-atomic Read-Modify-Write cycle.


LESENSE_StartDelaySet#

void LESENSE_StartDelaySet (uint8_t startDelay)

Set the start delay of the sensor interaction on each channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]startDelay

A number of LFACLK cycles to delay. A valid range: 0-3 (2 bit).

This function sets the start delay of the sensor interaction on each channel. It can be used for adjusting the start delay while running the application but it is also used by LESENSE_Init() for initialization.

Note

  • Users can configure the start delay by LESENSE_Init() function, but only with a significant overhead. This simple function serves the purpose of controlling this parameter after the channel has been configured. Be aware of the effects of the non-atomic Read-Modify-Write cycle.


LESENSE_ClkDivSet#

void LESENSE_ClkDivSet (LESENSE_ChClk_TypeDef clk, LESENSE_ClkPresc_TypeDef clkDiv)

Set the clock division for LESENSE timers.

Parameters
TypeDirectionArgument NameDescription
LESENSE_ChClk_TypeDef[in]clk

Select the clock to prescale.

  • lesenseClkHF - set AUXHFRCO clock divisor for HF timer.

  • lesenseClkLF - set LFACLKles clock divisor for LF timer.

LESENSE_ClkPresc_TypeDef[in]clkDiv

The clock divisor value. A valid range depends on the clk value.

Use this function to configure the clock division for the LESENSE timers used for excitation timing. The division setting is global but the clock source can be selected for each channel using LESENSE_ChannelConfig() function. See documentation for more details.

Note

  • If AUXHFRCO is used for excitation timing, LFACLK can't exceed 500 kHz. LFACLK can't exceed 50 kHz if the ACMP threshold level (ACMPTHRES) is not equal for all channels.


LESENSE_ChannelAllConfig#

void LESENSE_ChannelAllConfig (const LESENSE_ChAll_TypeDef * confChAll)

Configure all (16) LESENSE sensor channels.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_ChAll_TypeDef *[in]confChAll

A configuration structure for all (16) LESENSE sensor channels.

This function configures all sensor channels of the LESENSE interface. See the configuration parameter type definition (LESENSE_ChAll_TypeDef) for more details.

Note

  • Channels can be configured individually using LESENSE_ChannelConfig() function. Notice that pins used by the LESENSE module must be properly configured by the user explicitly for LESENSE to work as intended. (When configuring pins, consider the sequence of the configuration to avoid unintended pulses/glitches on output pins.)


LESENSE_ChannelConfig#

void LESENSE_ChannelConfig (const LESENSE_ChDesc_TypeDef * confCh, uint32_t chIdx)

Configure a single LESENSE sensor channel.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_ChDesc_TypeDef *[in]confCh

A configuration structure for a single LESENSE sensor channel.

uint32_t[in]chIdx

A channel index to configure (0-15).

This function configures a single sensor channel of the LESENSE interface. See the configuration parameter type definition (LESENSE_ChDesc_TypeDef) for more details.

Note

  • This function has been designed to minimize the effects of sensor channel reconfiguration while LESENSE is in operation. However, be aware of these effects and the right timing to call this function. Parameter useAltEx must be true in the channel configuration to use alternate excitation pins.


LESENSE_AltExConfig#

void LESENSE_AltExConfig (const LESENSE_ConfAltEx_TypeDef * confAltEx)

Configure the LESENSE alternate excitation modes.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_ConfAltEx_TypeDef *[in]confAltEx

A configuration structure for LESENSE alternate excitation pins.

This function configures the alternate excitation channels of the LESENSE interface. See the configuration parameter type definition (LESENSE_ConfAltEx_TypeDef) for more details.

Note

  • The useAltEx parameter must be true in the channel configuration structure (LESENSE_ChDesc_TypeDef) to use alternate excitation pins on the channel.


LESENSE_ChannelEnable#

void LESENSE_ChannelEnable (uint8_t chIdx, bool enaScanCh, bool enaPin)

Enable/disable LESENSE scan channel and the pin assigned to it.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chIdx

An identifier of the scan channel. A valid range: 0-15.

bool[in]enaScanCh

Enable/disable the selected scan channel by setting this parameter to true/false respectively.

bool[in]enaPin

Enable/disable the pin assigned to the channel selected by chIdx.

Use this function to enable/disable a selected LESENSE scan channel and the pin assigned to it.

Note

  • Users can enable/disable scan channels and the channel pin with the LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function controls these parameters after the channel has been configured.


LESENSE_ChannelEnableMask#

void LESENSE_ChannelEnableMask (uint16_t chMask, uint16_t pinMask)

Enable/disable LESENSE scan channel and the pin assigned to it.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]chMask

Set the corresponding bit to 1 to enable, 0 to disable the selected scan channel.

uint16_t[in]pinMask

Set the corresponding bit to 1 to enable, 0 to disable the pin on selected channel.

Use this function to enable/disable LESENSE scan channels and the pins assigned to them using a mask.

Note

  • Users can enable/disable scan channels and channel pins by using the LESENSE_ChannelAllConfig() function, but only with a significant overhead. This simple function controls these parameters after the channel has been configured.


LESENSE_ChannelTimingSet#

void LESENSE_ChannelTimingSet (uint8_t chIdx, uint8_t exTime, uint8_t sampleDelay, uint16_t measDelay)

Set LESENSE channel timing parameters.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chIdx

An identifier of the scan channel. A valid range is 0-15.

uint8_t[in]exTime

An excitation time on chIdx. The excitation will last exTime+1 excitation clock cycles. A valid range is 0-63 (6 bits).

uint8_t[in]sampleDelay

Sample delay on chIdx. Sampling will occur after sampleDelay+1 sample clock cycles. A valid range is 0-127 (7 bits).

uint16_t[in]measDelay

A measure delay on chIdx. Sensor measuring is delayed for measDelay+1 excitation clock cycles. A valid range is 0-127 (7 bits).

Use this function to set timing parameters on a selected LESENSE channel.

Note

  • Users can configure the channel timing parameters with the LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function controls these parameters after the channel has been configured.


LESENSE_ChannelThresSet#

void LESENSE_ChannelThresSet (uint8_t chIdx, uint16_t acmpThres, uint16_t cntThres)

Set LESENSE channel threshold parameters.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chIdx

An identifier of the scan channel. A valid range is 0-15.

uint16_t[in]acmpThres

ACMP threshold.

  • If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseDACIfData, acmpThres defines the 12-bit DAC data in the corresponding data register of the DAC interface (DACn_CH0DATA and DACn_CH1DATA). In this case, the valid range is 0-4095 (12 bits).

  • If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseACMPThres, acmpThres defines the 6-bit Vdd scaling factor of ACMP negative input (VDDLEVEL in ACMP_INPUTSEL register). In this case, the valid range is 0-63 (6 bits).

uint16_t[in]cntThres

A decision threshold for counter comparison. A valid range is 0-65535 (16 bits).

Use this function to set threshold parameters on a selected LESENSE channel.

Note

  • Users can configure the channel threshold parameters with the LESENSE_ChannelConfig() function, but only with a significant overhead. This simple function serves controls these parameters after the channel has been configured.


LESENSE_ChannelSlidingWindow#

void LESENSE_ChannelSlidingWindow (uint8_t chIdx, uint32_t windowSize, uint32_t initValue)

Configure a Sliding Window evaluation mode for a specific channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chIdx

An identifier of the scan channel. A valid range is 0-15.

uint32_t[in]windowSize

A window size to be used on all channels.

uint32_t[in]initValue

The initial sensor value for the channel.

This function will configure the evaluation mode, the initial sensor measurement (COMPTHRES), and the window size. For other channel-related configuration, see the LESENSE_ChannelConfig() function.

Warnings

  • Note that the step size and window size configuration are global to all LESENSE channels and use the same register field in the hardware. This means that any windowSize configuration passed to this function will apply for all channels and override all other stepSize/windowSize configurations.


LESENSE_ChannelStepDetection#

void LESENSE_ChannelStepDetection (uint8_t chIdx, uint32_t stepSize, uint32_t initValue)

Configure the step detection evaluation mode for a specific channel.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]chIdx

An identifier of the scan channel. A valid range is 0-15.

uint32_t[in]stepSize

A step size to be used on all channels.

uint32_t[in]initValue

The initial sensor value for the channel.

This function will configure the evaluation mode, the initial sensor measurement (COMPTHRES) and the window size. For other channel-related configuration, see the LESENSE_ChannelConfig() function.

Warnings

  • Note that the step size and window size configuration are global to all LESENSE channels and use the same register field in the hardware. This means that any stepSize configuration passed to this function will apply for all channels and override all other stepSize/windowSize configurations.


LESENSE_WindowSizeSet#

void LESENSE_WindowSizeSet (uint32_t windowSize)

Set the window size for all LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]windowSize

The window size to use for all channels.

The window size is used by all channels that are configured as lesenseEvalModeSlidingWindow.

Warnings

  • The window size configuration is using the same register field as the step detection size. As a result, the window size configuration will have an effect on channels configured with the lesenseEvalModeStepDetection evaluation mode as well.


LESENSE_StepSizeSet#

void LESENSE_StepSizeSet (uint32_t stepSize)

Set the step size for all LESENSE channels.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]stepSize

The step size to use for all channels.

The step size is configured using the same register field as used to configure window size. Therefore, calling this function will overwrite any previously configured window size as done by the LESENSE_WindowSizeSet() function.


LESENSE_DecoderStateAllConfig#

void LESENSE_DecoderStateAllConfig (const LESENSE_DecStAll_TypeDef * confDecStAll)

Configure all LESENSE decoder states.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_DecStAll_TypeDef *[in]confDecStAll

A configuration structure for all (16 or 32) LESENSE decoder states.

This function configures all the decoder states of the LESENSE interface. See the configuration parameter type definition (LESENSE_DecStAll_TypeDef) for more details.

Note

  • Decoder states can be configured individually using LESENSE_DecoderStateConfig() function. Starting from Series 2 Config 3 (xG23 and higher), this function configures a transition ARC instead of a decoder state.


LESENSE_DecoderStateConfig#

void LESENSE_DecoderStateConfig (const LESENSE_DecStDesc_TypeDef * confDecSt, uint32_t decSt)

Configure a single LESENSE decoder state.

Parameters
TypeDirectionArgument NameDescription
const LESENSE_DecStDesc_TypeDef *[in]confDecSt

A configuration structure for a single LESENSE decoder state.

uint32_t[in]decSt

A decoder state index to configure (0-15) or (0-31) depending on the device.

This function configures a single decoder state of the LESENSE interface. See the configuration parameter type definition (LESENSE_DecStDesc_TypeDef) for more details.

Note

  • Starting from Series 2 Config 3 (xG23 and higher), this function configures a transition ARC instead of a decoder state.


LESENSE_DecoderStateGet#

uint32_t LESENSE_DecoderStateGet (void )

Get the current state of the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • This function returns the value of the LESENSE_DECSTATE register that represents the current state of the LESENSE decoder.


LESENSE_DecoderPrsOut#

void LESENSE_DecoderPrsOut (bool enable, uint32_t decMask, uint32_t decVal)

Enable or disable the PRS output from the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

Enable/disable the PRS output from the LESENSE decoder. True to enable and false to disable.

uint32_t[in]decMask

A decoder state compare value mask.

uint32_t[in]decVal

A decoder state comparison value.


LESENSE_ScanStart#

void LESENSE_ScanStart (void )

Start scanning sensors.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


LESENSE_ScanStop#

void LESENSE_ScanStop (void )

Stop scanning sensors.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so the user should expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation in order to optimize an application.

  • If issued during a scan, the command takes effect after scan completion.


LESENSE_DecoderStart#

void LESENSE_DecoderStart (void )

Start the LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


LESENSE_ResultBufferClear#

void LESENSE_ResultBufferClear (void )

Clear the result buffer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function will wait for any pending previous write operation to the CMD register to complete before accessing the CMD register. It will also wait for the write operation to the CMD register to complete before returning. Each write operation to the CMD register may take up to 3 LF clock cycles, so expect some delay. The user may implement a separate function to write multiple command bits in the CMD register in one single operation to optimize an application.


LESENSE_Reset#

void LESENSE_Reset (void )

Reset the LESENSE module.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Use this function to reset LESENSE registers.

Note

  • Resetting LESENSE registers is required in each reset or power-on cycle to configure the default values of the RAM mapped LESENSE registers. LESENSE_Reset() can be called on initialization by setting the reqReset parameter to true in LESENSE_Init(). Starting from Series 2 Config 3 (xG23 and higher), this function leaves LESENSE in the disabled state.


LESENSE_DecoderStop#

void LESENSE_DecoderStop (void )

Stop LESENSE decoder.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Disables LESENSE decoder by setting the command to LESENSE_DECCTRL register.


LESENSE_StatusGet#

uint32_t LESENSE_StatusGet (void )

Get the current status of LESENSE.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_STATUS register that contains the OR combination of the following status bits for EFR series 0/1:

    • LESENSE_STATUS_BUFDATAV - Result data valid. Set when data is available in result buffer. Cleared when buffer is empty.

    • LESENSE_STATUS_BUFFULL - Result buffer full. Set when result buffer is full.

    • LESENSE_STATUS_BUFHALFFULL - Result buffer half full. Set when result buffer is half full.

    • LESENSE_STATUS_RUNNING - LESENSE is active.

    • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

    The OR combination of the following status bits for EFR series 2:

    • LESENSE_STATUS_RESFIFOV - Result Fifo valid. Set when data is available in result Fifo. Cleared when Fifo is empty.

    • LESENSE_STATUS_RESFIFOFULL - Result Fifo full. Set when result Fifo is full.

    • LESENSE_STATUS_RUNNING - LESENSE is active.

    • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

    • LESENSE_STATUS_FLUSHING - Fifo flushing

    • LESENSE_STATUS_READBUSY - Fifo Read busy


LESENSE_StatusWait#

void LESENSE_StatusWait (uint32_t flag)

Wait until status of LESENSE is equal to what was requested.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flag

The OR combination of the following status bits for EFR series 0/1:

  • LESENSE_STATUS_BUFDATAV - Result data valid. Set when data is available in result buffer. Cleared when buffer is empty.

  • LESENSE_STATUS_BUFHALFFULL - Result buffer half full. Set when result buffer is half full.

  • LESENSE_STATUS_BUFFULL - Result buffer full. Set when result buffer is full.

  • LESENSE_STATUS_RUNNING - LESENSE is active.

  • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

  • LESENSE_STATUS_DACACTIVE - The DAC interface is currently active.

The OR combination of the following status bits for EFR series 2:

  • LESENSE_STATUS_RESFIFOV - Result FIFO valid. Set when data is available in result FIFO. Cleared when FIFO is empty.

  • LESENSE_STATUS_RESFIFOFULL - Result FIFO full. Set when result FIFO is full.

  • LESENSE_STATUS_RUNNING - LESENSE is active.

  • LESENSE_STATUS_SCANACTIVE - LESENSE is currently interfacing sensors.

  • LESENSE_STATUS_FLUSHING - FIFO flushing

  • LESENSE_STATUS_READBUSY - FIFO Read busy

Polls LESENSE_STATUS register and waits until requested combination of flags are set.


LESENSE_ChannelActiveGet#

uint32_t LESENSE_ChannelActiveGet (void )

Get the currently active channel index.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_CHINDEX register that contains the index of currently active channel (0-15).


LESENSE_ScanResultGet#

uint32_t LESENSE_ScanResultGet (void )

Get the latest scan comparison result (1 bit / channel).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of the LESENSE_SCANRES register that contains the comparison result of last scan on all channels. Bit x is set if a comparison triggered on channel x, which means that LESENSE counter met the comparison criteria set in LESENSE_CHx_EVAL by COMPMODE and CNTTHRES.


LESENSE_ScanResultDataGet#

uint32_t LESENSE_ScanResultDataGet (void )

Get the oldest unread data from the result buffer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Make sure that the STORERES bit is set in LESENSE_CHx_EVAL, or the STRSCANRES bit is set in LESENSE_CTRL; otherwise, returns the undefined value.

Returns

  • Returns the value of LESENSE_RESDATA register that contains the oldest unread counter result from result buffer.


LESENSE_SensorStateGet#

uint32_t LESENSE_SensorStateGet (void )

Get the current state of the LESENSE sensor.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the value of LESENSE_SENSORSTATE register that represents the current state of the LESENSE sensor.


LESENSE_IntClear#

void LESENSE_IntClear (uint32_t flags)

Clear one or more pending LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Pending LESENSE interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


LESENSE_IntEnable#

void LESENSE_IntEnable (uint32_t flags)

Enable one or more LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to enable. Use a set of interrupt flags OR-ed together to enable multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


LESENSE_IntDisable#

void LESENSE_IntDisable (uint32_t flags)

Disable one or more LESENSE interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources of LESENSE module (LESENSE_IF_nnn).


LESENSE_IntSet#

void LESENSE_IntSet (uint32_t flags)

Set one or more pending LESENSE interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

LESENSE interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources of LESENSE module (LESENSE_IFS_nnn).


LESENSE_IntGet#

uint32_t LESENSE_IntGet (void )

Get pending LESENSE interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Event bits are not cleared by the use of this function.

Returns

  • Pending LESENSE interrupt sources. The OR combination of valid interrupt flags of the LESENSE module (LESENSE_IF_nnn).


LESENSE_IntGetEnabled#

uint32_t LESENSE_IntGetEnabled (void )

Get enabled and pending LESENSE interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Event bits are not cleared by the use of this function.

Returns

  • Pending and enabled LESENSE interrupt sources. Return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in LESENSE_IEN_nnn register (LESENSE_IEN_nnn) and

    • the OR combination of valid interrupt flags of LESENSE module (LESENSE_IF_nnn).


Macro Definition Documentation#

LESENSE_NUM_DECODER_STATES#

#define LESENSE_NUM_DECODER_STATES
Value:
(_LESENSE_DECSTATE_DECSTATE_MASK + 1)

Number of decoder states supported by current device.


LESENSE_NUM_ARCS#

#define LESENSE_NUM_ARCS
Value:
(LESENSE_NUM_DECODER_STATES << 1)

Number of ARCs supported by current device.

Number of ARCS is the number of states times 2


LESENSE_NUM_CHANNELS#

#define LESENSE_NUM_CHANNELS
Value:
16

Number of LESENSE channels.


LESENSE_CORECTRL_DESC_DEFAULT#

#define LESENSE_CORECTRL_DESC_DEFAULT
Value:
{ \
lesenseScanStartPeriodic,/* Start new scan each time the period counter overflows. */ \
lesensePRSCh0, /* Default PRS channel is selected. */ \
lesenseScanConfDirMap, /* Direct mapping SCANCONF register usage strategy. */ \
false, /* Do not invert ACMP0 output. */ \
false, /* Do not invert ACMP1 output. */ \
false, /* Disable dual sampling. */ \
true, /* Store scan result after each scan. */ \
15u, /* Default value for the FIFO trigger level */ \
lesenseDMAWakeUpDisable, /* Do not wake up on DMA from EM2. */ \
true /* Keep LESENSE running in debug mode. */ \
}

Default configuration for LESENSE_CtrlDesc_TypeDef structure.


LESENSE_TIMECTRL_DESC_DEFAULT#

#define LESENSE_TIMECTRL_DESC_DEFAULT
Value:
{ \
0U, /* No sensor interaction delay. */ \
false /* Do not delay the AUXHFRCO startup. */ \
}

Default configuration for LESENSE_TimeCtrlDesc_TypeDef structure.


LESENSE_PERCTRL_DESC_DEFAULT#

#define LESENSE_PERCTRL_DESC_DEFAULT
Value:
{ \
lesenseDACIfData, /* DAC channel 0 data is defined by DAC_CH0DATA register. */ \
lesenseACMPModeMuxThres, /* LESENSE controls input mux and threshold value of ACMP0. */ \
lesenseACMPModeMuxThres, /* LESENSE controls input mux and threshold value of ACMP1. */ \
false, /* DAC is enabled for before every channel measurement. */ \
false, /* DAC is enabled a full clock cycle before sensor interaction */ \
}

Default configuration for LESENSE_PerCtrl_TypeDef structure.


LESENSE_DECCTRL_DESC_DEFAULT#

#define LESENSE_DECCTRL_DESC_DEFAULT
Value:
{ \
false, /* Disable check of current state. */ \
true, /* Enable channel x % 16 interrupt on state x change. */ \
true, /* Enable decoder hysteresis on PRS0 output. */ \
true, /* Enable decoder hysteresis on PRS1 output. */ \
true, /* Enable decoder hysteresis on PRS2 output. */ \
true, /* Enable decoder hysteresis on PRS3 output. */ \
false, /* Disable count mode on decoder PRS channels 0 and 1*/ \
}

Default configuration for LESENSE_PerCtrl_TypeDef structure.


LESENSE_INIT_DEFAULT#

#define LESENSE_INIT_DEFAULT
Value:
{ \
.coreCtrl = LESENSE_CORECTRL_DESC_DEFAULT, /* Default core control parameters. */ \
.timeCtrl = LESENSE_TIMECTRL_DESC_DEFAULT, /* Default time control parameters. */ \
.perCtrl = LESENSE_PERCTRL_DESC_DEFAULT, /* Default peripheral control parameters. */ \
.decCtrl = LESENSE_DECCTRL_DESC_DEFAULT /* Default decoder control parameters. */ \
}

Default configuration for LESENSE_Init_TypeDef structure.


LESENSE_CH_CONF_DEFAULT#

#define LESENSE_CH_CONF_DEFAULT
Value:
{ \
false, /* Disable scan channel. */ \
false, /* Disable assigned pin on scan channel. */ \
false, /* Disable interrupts on channel. */ \
lesenseChPinExDis, /* Channel pin is disabled during excitation period. */ \
lesenseChPinIdleDis, /* Channel pin is disabled during idle period. */ \
false, /* Do not use alternate excitation pins for excitation. */ \
false, /* Disabled to shift results from this channel to decoder register. */ \
false, /* Disabled to invert scan result bit. */ \
lesenseStoreSampleDisable,/* Disabled to store counter value in result buffer. */ \
lesenseClkLF, /* Use LF clock for excitation timing. */ \
lesenseClkLF, /* Use LF clock for sample timing. */ \
0x00U, /* Excitation time is set to 0(+1) excitation clock cycles. */ \
0x00U, /* Sample delay is set to 0(+1) sample clock cycles. */ \
0x00U, /* Measure delay is set to 0 excitation clock cycles.*/ \
0x00U, /* ACMP threshold has been set to 0. */ \
lesenseSampleModeACMP, /* ACMP output will be used in comparison. */ \
lesenseSetIntNone, /* No interrupt is generated by the channel. */ \
0x00U, /* Counter threshold has bee set to 0x00. */ \
lesenseCompModeLess, /* Compare mode has been set to trigger interrupt on "less". */ \
lesenseEvalModeThreshold, /* Evaluation mode has been set to trigger interrupt on threshold. */ \
0x00U /* No offset for IADC or ACMP interaction. */ \
}

Default configuration for the scan channel.


LESENSE_SCAN_CONF_DEFAULT#

#define LESENSE_SCAN_CONF_DEFAULT
Value:
{ \
{ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 0. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 1. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 2. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 3. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 4. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 5. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 6. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 7. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 8. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 9. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 10. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 11. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 12. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 13. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 14. */ \
LESENSE_CH_CONF_DEFAULT, /* Scan channel 15. */ \
} \
}

Default configuration for all the sensor channels.


LESENSE_ALTEX_CH_CONF_DEFAULT#

#define LESENSE_ALTEX_CH_CONF_DEFAULT
Value:
{ \
false /* Alternate excitation disabled.*/ \
}

Default configuration for the alternate excitation channel.


LESENSE_ALTEX_CONF_DEFAULT#

#define LESENSE_ALTEX_CONF_DEFAULT
Value:
{ \
{ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 0. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 1. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 2. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 3. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 4. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 5. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 6. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 7. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 8. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 9. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 10. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 11. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 12. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 13. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT, /* Alternate excitation channel 14. */ \
LESENSE_ALTEX_CH_CONF_DEFAULT /* Alternate excitation channel 15. */ \
} \
}

Default configuration for all the alternate excitation channels.


LESENSE_ST_CONF_DEFAULT#

#define LESENSE_ST_CONF_DEFAULT
Value:
{ \
0x0FU, /* Compare value set to 0x0F. */ \
0x00U, /* All decoder inputs masked. */ \
0U, /* Current state must be state 0. */ \
0U, /* Next state is state 0. */ \
lesenseTransActNone, /* No PRS action performed on compare match. */ \
false /* No interrupt triggered on compare match. */ \
}

Default configuration for the decoder state condition.


LESENSE_DECODER_CONF_DEFAULT#

#define LESENSE_DECODER_CONF_DEFAULT

Default configuration for all decoder states.