EMLIB to Peripheral HAL Migration Guide: Considerations#
Migration Considerations#
Coexistence:
Both libraries can coexist during migration for Series 2
This should be avoided in the long run to reduce code size
No direct compatibility layer available
Code Changes Required:
API calls require modification (not just renaming)
Initialization sequences need restructuring
Clock management must be handled explicitly
Testing Requirements:
Behavioral equivalence testing essential
Register-level verification recommended
Consider incremental migration approach
Integration testing with full system
When to Migrate#
Migrate now if:
Starting a new Series 3 project (required)
Beginning a new Series 2 project (recommended)
Adding significant new peripheral functionality
Refactoring existing peripheral code
Planning long-term product lifecycle
Consider delaying if:
Stable Series 0/1/2 product with no Series 3 plans
Limited development resources
Near end-of-life for existing product
No significant new features planned
Incremental Migration:
Migrate peripheral-by-peripheral
Start with least complex peripherals
Test thoroughly between migrations
Maintain regression test suite