You are viewing documentation for version:
PDFFont definition structure.
Public Attributes#
void *
Pointer to the pixel map for the font.
uint16_t
Number of elements in the font pixel map.
uint8_t
Size of each element in the font pixel map.
uint8_t
Width in pixels of each character.
uint8_t
Height in pixels of each character.
uint8_t
Number of pixels between each line in this font.
uint8_t
Number of pixels between each character in this font.
The font class is used to tell glib if the font contains numbers only or characters and numbers.
Public Attribute Documentation#
pFontPixMap#
void* GLIB_Font_t::pFontPixMap
Pointer to the pixel map for the font.
cntOfMapElements#
uint16_t GLIB_Font_t::cntOfMapElements
Number of elements in the font pixel map.
sizeOfMapElement#
uint8_t GLIB_Font_t::sizeOfMapElement
Size of each element in the font pixel map.
fontRowOffset#
uint8_t GLIB_Font_t::fontRowOffset
Font row offset.
fontWidth#
uint8_t GLIB_Font_t::fontWidth
Width in pixels of each character.
fontHeight#
uint8_t GLIB_Font_t::fontHeight
Height in pixels of each character.
lineSpacing#
uint8_t GLIB_Font_t::lineSpacing
Number of pixels between each line in this font.
charSpacing#
uint8_t GLIB_Font_t::charSpacing
Number of pixels between each character in this font.
fontClass#
GLIB_Font_Class GLIB_Font_t::fontClass
The font class is used to tell glib if the font contains numbers only or characters and numbers.