CRC initialization structure.

Public Attributes#

bool

Reverse byte order.

bool

Reverse bits within each input byte.

bool

Enable/disable byte mode.

bool

Enable automatic initialization by re-seeding the CRC result based on the init value after reading one of the CRC data registers.

uint32_t

CRC polynomial value.

uint32_t

CRC initialization value.

Public Attribute Documentation#

reverse_byte_order#

bool sl_hal_gpcrc_init_t::reverse_byte_order

Reverse byte order.

This has an effect when sending a 32-bit word or 16-bit half word input to the CRC calculation. When set to true, the input bytes are reversed before entering the CRC calculation. When set to false, the input bytes stay in the same order.


reverse_bits#

bool sl_hal_gpcrc_init_t::reverse_bits

Reverse bits within each input byte.

This setting enables or disables byte level bit reversal. When byte-level bit reversal is enabled, then each byte of input data will be reversed before entering CRC calculation.


enable_byte_mode#

bool sl_hal_gpcrc_init_t::enable_byte_mode

Enable/disable byte mode.

When byte mode is enabled, then all input is treated as single byte input even though the input is a 32-bit word or a 16-bit half word. Only the least significant byte of the data-word will be used for CRC calculation for all writes.


auto_init#

bool sl_hal_gpcrc_init_t::auto_init

Enable automatic initialization by re-seeding the CRC result based on the init value after reading one of the CRC data registers.


crc_poly#

uint32_t sl_hal_gpcrc_init_t::crc_poly

CRC polynomial value.

GPCRC supports either a fixed 32-bit polynomial or a user-configurable 16 bit polynomial. The fixed 32-bit polynomial is the one used in IEEE 802.3, which has the value 0x04C11DB7. To use the 32-bit fixed polynomial, assign 0x04C11DB7 to the crc_poly field. To use a 16-bit polynomial, assign a value to crc_poly where the upper 16 bits are zero.

The polynomial should be written in normal bit order. For instance, to use the CRC-16 polynomial X^16 + X^15 + X^2 + 1, first convert it to hex representation and remove the highest order term of the polynomial. This will give 0x8005 as the value to write into crcPoly.


init_value#

uint32_t sl_hal_gpcrc_init_t::init_value

CRC initialization value.

This value is assigned to the GPCRC_INIT register. The initValue is loaded into the data register when calling the sl_hal_gpcrc_start function or when one of the data registers are read while auto_init is enabled.