You are viewing documentation for version:
BURTC initialization structure. 
Public Attributes#
uint32_t
Clock divider. Supported range is 1-32768. 
bool
If true, counter will keep running under debug halt. 
bool
Set if Compare Value 0 is also top value (counter restart) 
bool
Enable EM4 wakeup on compare match. 
bool
Enable EM4 wakeup on counter overflow. 
Public Attribute Documentation#
clock_divider#
uint32_t sl_hal_burtc_init_t::clock_divider
Clock divider. Supported range is 1-32768. 
debug_run#
bool sl_hal_burtc_init_t::debug_run
If true, counter will keep running under debug halt. 
compare0_top#
bool sl_hal_burtc_init_t::compare0_top
Set if Compare Value 0 is also top value (counter restart) 
em4_comparator#
bool sl_hal_burtc_init_t::em4_comparator
Enable EM4 wakeup on compare match. 
em4_overflow#
bool sl_hal_burtc_init_t::em4_overflow
Enable EM4 wakeup on counter overflow.