Power Manager Appendix#
Glossary#
Energy Mode (EM): Hardware power state (EM0=active, EM1=sleep, EM2=deep sleep, EM3=stop, EM4=shutoff)
EM1P: Subset of EM1 enabling radio operation while the core and high-speed peripherals are powered down. Entered when radio is active and EM2 is requested. Core sleeps, but HFXO and radio (RX only) remain active.
Requirement: Software constraint preventing sleep deeper than specified energy mode
Schedule Wake-up: Planned wake-up event with timing optimization
Pin Retention: Feature maintaining GPIO pin states through EM4 reset
HFXO: High Frequency Crystal Oscillator (external high-precision clock source)
LFRCO: Low Frequency RC Oscillator
Universal Configurator (UC): GUI-based configuration tool
API: Application Programming Interface
Related Documentation
Power Manager API Reference - Complete API documentation with function signatures, parameters, and return values
Clock Manager Documentation - Essential companion for oscillator configuration
Energy Profiler User Guide - Advanced power consumption analysis tool
HFXO Manager Documentation - Series 2 specific crystal oscillator management
Simplicity Studio 5 User Guide - Complete IDE documentation
Simplicity Studio 6 User Guide - Complete IDE documentation
Sleep Timer Documentation - Critical for low-power timer management and schedule wake-up optimization
Extended Examples#
Using Event Notifications#
#include "sl_power_manager.h"
static sl_power_manager_em_transition_event_handle_t power_event_handle;
void my_power_transition_callback(sl_power_manager_em_t from, sl_power_manager_em_t to) {
if (from < to && to >= SL_POWER_MANAGER_EM2) {
save_application_context();
} else if (from > to && from >= SL_POWER_MANAGER_EM2) {
restore_application_context();
}
}
void app_init(void) {
sl_power_manager_em_transition_event_info_t event_info = {
.event_mask = (SL_POWER_MANAGER_EVENT_TRANSITION_ENTERING_EM2 | SL_POWER_MANAGER_EVENT_TRANSITION_LEAVING_EM2),
.on_event = my_power_transition_callback
};
// When entering or exiting EM2, call the callback to manage the application context
sl_power_manager_subscribe_em_transition_event(&power_event_handle, &event_info);
}Schedule Wake-up Tuning#
#include "sl_power_manager.h"
// Battery-optimized configuration
void configure_for_battery_life(void)
{
// Allow later early wake-up for power savings (risk: potential to be late for scheduled events)
sl_power_manager_schedule_wakeup_set_restore_overhead_tick(-5);
// Prevent frequent short deep sleep cycles
sl_power_manager_schedule_wakeup_set_minimum_offtime_tick(30);
}Execution Modes (Series 3 Only)#
#include "sl_power_manager.h"
// Optimize for Series 3 execution modes
void configure_series3_power_optimization(void)
{
// Add performance requirement when high processing needed
sl_power_manager_add_performance_mode_requirement();
// Do some intensive processing...
// Remove when returning to standard execution
sl_power_manager_remove_performance_mode_requirement();
// Series 3 automatically manages SYSCLK switching (SOCPLL ↔ HFXO)
// Power Manager coordinates with 36μs SOCPLL lock time
}FAQ#
Q: When should I add a requirement on an energy mode?
A: Add EM1 requirements when your module needs immediate responsiveness or high-frequency clocks (UART high baud rates, precise timing, interrupt latency <1μs). Adding requirements for other energy modes does nothing and serves no purpose:
EM0 requirements: Meaningless since EM0 is the active state, not a sleep mode
EM2 requirements: The hardware automatically manages EM2/EM3 subdomains based on peripheral usage
EM3 requirements: The Power Manager cannot decide to enter EM4 without an explicit call to
sl_power_manager_enter_em4(), so EM3 requirements are unnecessaryEM4 requirements: Meaningless since EM4 is the lowest energy mode
Q: How does pin retention work in EM4?
A: Configure SL_POWER_MANAGER_INIT_EMU_EM4_PIN_RETENTION_MODE, set pin states before EM4 entry, and call sl_power_manager_em4_unlatch_pin_retention() after reset to release pins back to peripheral control.
Q: What happens if I remove a requirement I never added?
A: This creates undefined behavior. Always track requirement state in your module and only remove requirements you have added.
Q: Why is my system consuming more power than expected?
A: Common causes include: persistent EM1 requirements preventing deep sleep, UART/SPI drivers blocking sleep, GPIO leakage current, unused peripheral clocks enabled, or voltage scaling disabled. Use sl_power_manager_debug_print_em_requirements() to identify active requirements.
Q: What's the difference between EM2 and EM3?
A: Starting with Series 2 devices, EM2 and EM3 have been merged. The EMU hardware automatically powers down as many subdomains as possible. To reach EM3 power levels, peripherals must be disabled.
Q: When should I use EM4 vs EM2/EM3?
A: Use EM4 for ultra-low power when you can tolerate system reset on wake-up and have long sleep periods. Use EM2/EM3 for applications needing faster wake-up and preserved RAM state.
Q: How does Power Manager work with RTOS?
A: With FreeRTOS or Micrium OS, Power Manager automatically handles sleep in the OS idle task. Do not call sl_power_manager_sleep() manually. The system enters the lowest allowable energy mode when all tasks are blocked.
Q: How do I preserve data across EM4 resets?
A: Use Backup RAM (BURAM) registers to store critical data. BURAM survives EM4 resets while regular RAM is lost. Copy data to/from BURAM->RET[] before EM4 entry and after wake-up.