Silicon Labs
gecko-platform/latest/service/api/structsl-se-command-context-t
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
Results 1-5 of 5 for gecko-platform/latest/service/api/structsl-se-command-context-t in 0.19 seconds
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
Training ... Register // Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... Definition at line 54 of file platform/service/sleeptimer/inc/sl_sleeptimer.h
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Core API, inititalizing of SE Manager and SE command context (Core) ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE Manager is waiting for the ...
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollers Resource TypeSoftware API documentation
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
Command Line Interface (CLI) + CLI Storage Device Initialization (EMU, CMU) ... Platform Services Detail Device Initialization ... platform/latest/service/api/group-power-manager
AN1247: Anti-Tamper Protection Configuration and Use
https://www.silabs.com/.../an1247-efr32-secure-vault-tamper....
SE temperature is monitored to be within 5 degrees C of the limits for the device. ... command (4 bytes) Tamper disable mask (4 bytes) Access certificate (156 bytes) Disable tamper command ...
Resource TypeApplication Notes
    Results 1-5 of 5 for gecko-platform/latest/service/api/structsl-se-command-context-t