Silicon Labs
gecko-platform/middleware/api/struct-u-s-b-device-descriptor-type-def
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
Results 1-5 of 5 for gecko-platform/middleware/api/struct-u-s-b-device-descriptor-type-def in 0.13 seconds
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... .h source files for the SLEEPTIMER device driver library are in the service/ ... All API functions can be called from within interrupt handlers.
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
You are viewing documentation for version: 4.2 | Version History ... Please refer to Segger's documentation for further information on RTT. ... You should avoid using it in production.
ProductMicrocontrollers Resource TypeSoftware API documentation
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
P L AT F O R M A N D M C U A P P S | N O V E M B E R 2 0 2 0 ... Gecko Platform –EMLIB Peripheral Library ... Device Init component adds autogen files and function calls to project:
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
Configuration Options The API Flow Control Support ... [in] type Abort type – whether to abort only Tx, only Rx, or both. ... The UARTDRV device handle used to start the transfer.
ProductMicrocontrollers Resource TypeSoftware API documentation
    Results 1-5 of 5 for gecko-platform/middleware/api/struct-u-s-b-device-descriptor-type-def