You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
Core API, inititalizing of SE Manager and SE command context (Core) ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE Manager is waiting for the ...
// Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... All API functions can be called from within interrupt handlers. ... 0 = highest priority. uint16_t N/A
Threading primitive implementation for mbed TLS. This file contains the glue logic between the mbed TLS threading API and two RTOS'es supported, being Micrium OS and FreeRTOS. ... Note
ProductMicrocontrollersResource TypeSoftware API documentation