Training ... Register // Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... Definition at line 73 of file platform/service/sleeptimer/inc/sl_sleeptimer.h
// Platform//Version 5.0.1 //Security ... Devices with the SE subsystem includes a low level crypto API where the SE Manager will use the SE hardware peripherals to accelerate cryptographic ...
... document can be found at https://docs.silabs.com/gecko-platform/latest/service/api/group-sl-se-manager. ... SE temperature is monitored to be within 5 degrees C of the limits for the device.
... a special Energy Mode to maintain the debug capabilities and the power consumption will ... Functions sl_status_t sl_iostream_rtt_init (void) ... Returns Status result Variable Documentation
ProductMicrocontrollersResource TypeSoftware API documentation