TensorFlow Lite Micro Debug#

Additional SL utilities for logging in TensorFlow Lite Micro.

Functions#

void

Enable or disable debug logging.

bool

Check if debug logging is enabled.

Function Documentation#

sl_tflite_micro_enable_debug_log#

void sl_tflite_micro_enable_debug_log (bool enable)

Enable or disable debug logging.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

Whether the debug logging should be enabled or disabled.


sl_tflite_micro_is_debug_log_enabled#

bool sl_tflite_micro_is_debug_log_enabled (void )

Check if debug logging is enabled.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Whether debug logging is enabled.