TensorFlow Lite Micro Debug#
Additional SL utilities for logging in TensorFlow Lite Micro.
Functions#
void
sl_tflite_micro_enable_debug_log(bool enable)
Enable or disable debug logging.
bool
Check if debug logging is enabled.
Function Documentation#
sl_tflite_micro_enable_debug_log#
void sl_tflite_micro_enable_debug_log (bool enable)
Enable or disable debug logging.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | Whether the debug logging should be enabled or disabled. |
sl_tflite_micro_is_debug_log_enabled#
bool sl_tflite_micro_is_debug_log_enabled (void )
Check if debug logging is enabled.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Whether debug logging is enabled.