Feature Generators#

This guide describes how to add and configure feature generator components in a machine learning project. Feature generators convert raw sensor data into the input format which a model expects. This document covers the Audio Feature Generator (fe_audio) for microphone-based classification models.


1. Add the Audio Feature Generator Component#

For microphone-based classification models, add the Audio Feature Generator component ( fe_audio ) to convert audio into spectrogram features for inference. Image, IMU, and other non-audio models do not require this component.

Add one fe_audio component instance per audio model. Each instance name must match the corresponding ML Model ( ml_model ) instance name.

In Simplicity Studio#

Perform the following steps in Simplicity Studio.

  1. Open the project .slcp file and select the SOFTWARE COMPONENTS tab.

  2. Navigate to Silicon Labs AI/ML → Machine Learning → Feature Generator, select Audio Feature Generator ( fe_audio ), and then click Install.

Install the Audio Feature Generator componentInstall the Audio Feature Generator component

  1. When prompted, enter an instance name that matches the corresponding ml_model instance (for example, keyword_spotting).

Create an Audio Feature Generator component instanceCreate an Audio Feature Generator component instance

  1. After installation, select the instance under Audio Feature Generator and click Configure to open its settings (see Section 2).

Open the installed Audio Feature Generator instance configurationOpen the installed Audio Feature Generator instance configuration

Repeat steps 2 to 4 for each audio model in the project.

When editing the .slcp file directly, the component entries look like this:

component:
  - id: fe_audio
    instance:
      - keyword_spotting

2. Configure Audio Frontend Parameters#

The audio frontend converts microphone samples into the int8 features required by the model. Configure these settings to match the settings used during model training.

In Simplicity Studio#

Perform the following steps in Simplicity Studio.

  1. Open the Audio Feature Generator instance in Software Components to review frontend settings. The configuration UI has two groups, shown below for a keyword_spotting instance:Audio Feature Generator configuration for keyword_spottingAudio Feature Generator configuration for keyword_spotting

  • Configurable parameters: Instance options that you can change using the graphical user interface (GUI), such as Audio Gain. The values you set are written into the generated sl_fe_audio_<instance>_config.h and used during the build process.

  • Model defined parameters (read-only, from trained .tflite): Frontend settings from the matching audio model (sample rate, window timing, filterbank settings, and similar). When a value is not embedded in the model, the build uses built-in defaults. Keep the model-provided values unchanged so that inference remains aligned with trained values.

  1. Enable parameter-header generation in the matching ml_model instance's .mlconf so that the MVP Compiler exports frontend metadata from the .tflite:

    model: tflite/keyword_spotting.tflite
    codegen:
      model_parameters_header:
        enabled: true

    The fe_audio instance name must match the ml_model instance name (for example, both keyword_spotting). After project generation, the audio frontend uses the model-specific values from <instance>_generated_parameters.h (for example, keyword_spotting_generated_parameters.h).


3. Audio Feature Generation API#

For initialization, feature updates, filling input tensors, and platform-specific behavior, see the ML Audio Feature Generation API reference.


4. Multiple Audio Configurations#

A project with more than one audio model needs a separate fe_audio instance (and matching ml_model instance) for each model.

Declare Instances in the Project#

Add one fe_audio instance per audio model in Simplicity Studio or .slcp (see Section 1). Simplicity Studio generates a matching sl_fe_audio_<instance>_cfg for each instance in autogen/sl_fe_audio_instances.h and autogen/sl_fe_audio_instances.c.

Switch Between Configurations at Runtime#

Only one audio frontend is active at a time. To move from one model's configuration to another:

  1. Call sl_ml_audio_feature_generation_deinit() to stop the current frontend.

  2. Call sl_ml_audio_feature_generation_init(&sl_fe_audio_<instance>_cfg) with the next instance's config struct.

Example:

sl_ml_audio_feature_generation_init(&sl_fe_audio_first_model_cfg);
/* ... run inference with the first audio model ... */
sl_ml_audio_feature_generation_deinit();
sl_ml_audio_feature_generation_init(&sl_fe_audio_second_model_cfg);
/* ... run inference with the second audio model ... */

See the ML Audio Feature Generation API reference for function details.


5. Example Applications#

Application

Boards

Models

Voice control (keyword spotting)

Silicon Labs boards

One audio model

See the AI/ML Sample Applications documentation for voice-control example projects you can create in Simplicity Studio.