IMU - Inertial Measurement Unit#
Inertial Measurement Unit driver.
Inertial Measurement Unit driver.
IMU example code#
Basic example for looping measurement of orientation data:
#include "sl_imu.h"
int main( void )
{
...
int16_t o_vec[3];
sl_imu_init();
// Configure sample rate
sl_imu_configure(10);
// Recalibrate gyro
sl_imu_calibrate_gyro();
while (true) {
sl_imu_update();
while (!sl_imu_is_data_ready()) {
// wait
}
sl_imu_get_orientation(o_vec);
...
}
} Modules#
State Definitions#
The IMU is disabled
The IMU is fully configured and ready to take measurements
The IMU is being initialized
The IMU is being calibrated
Functions#
Initialize and calibrate the IMU chip.
De-initialize the IMU chip.
Return IMU state.
Get a new set of data from the accel and gyro sensor and updates the fusion calculation.
Reset the fusion calculation.
Retrieve the processed acceleration data.
Retrieve the processed orientation data.
Retrieve the processed gyroscope data.
Perform gyroscope calibration to cancel gyro bias.
Retrieve the processed gyroscope correction angles.
Configure the IMU.
Check if new accel/gyro data is available for read.
Retrieve the raw acceleration data from the IMU.
Retrieve the raw gyroscope data from the IMU.
State Definitions Documentation#
Function Documentation#
sl_imu_init#
sl_status_t sl_imu_init (sl_ssi_handle_t ssi_driver_handle)
Initialize and calibrate the IMU chip.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ssi_handle_t | N/A | ssi_driver_handle |
Returns
Returns zero on OK, non-zero otherwise
sl_imu_deinit#
sl_status_t sl_imu_deinit (void )
De-initialize the IMU chip.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Returns zero on OK, non-zero otherwise
sl_imu_get_state#
uint8_t sl_imu_get_state (void )
Return IMU state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
IMU state
sl_imu_update#
void sl_imu_update (void )
Get a new set of data from the accel and gyro sensor and updates the fusion calculation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_imu_reset#
void sl_imu_reset (void )
Reset the fusion calculation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_imu_get_acceleration#
void sl_imu_get_acceleration (int16_t avec)
Retrieve the processed acceleration data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int16_t | [out] | avec | Three dimensional acceleration vector |
sl_imu_get_orientation#
void sl_imu_get_orientation (int16_t ovec)
Retrieve the processed orientation data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int16_t | [out] | ovec | Three dimensional orientation vector |
sl_imu_get_gyro#
void sl_imu_get_gyro (int16_t gvec)
Retrieve the processed gyroscope data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int16_t | [out] | gvec | Three dimensional gyro vector |
sl_imu_calibrate_gyro#
sl_status_t sl_imu_calibrate_gyro (sl_ssi_handle_t ssi_driver_handle)
Perform gyroscope calibration to cancel gyro bias.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ssi_handle_t | N/A | ssi_driver_handle |
sl_imu_get_gyro_correction_angles#
void sl_imu_get_gyro_correction_angles (float acorr)
Retrieve the processed gyroscope correction angles.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [out] | acorr | Three dimensional gyro correction angle vector |
sl_imu_configure#
void sl_imu_configure (float sampleRate, sl_ssi_handle_t ssi_driver_handle)
Configure the IMU.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [in] | sampleRate | The desired sample rate of the acceleration and gyro sensor |
| sl_ssi_handle_t | N/A | ssi_driver_handle |
sl_imu_is_data_ready#
bool sl_imu_is_data_ready (sl_ssi_handle_t ssi_driver_handle)
Check if new accel/gyro data is available for read.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ssi_handle_t | N/A | ssi_driver_handle |
Returns
True if the measurement data is ready, false otherwise
sl_imu_get_acceleration_raw_data#
void sl_imu_get_acceleration_raw_data (float avec)
Retrieve the raw acceleration data from the IMU.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [out] | avec | Three dimensional raw acceleration vector |
sl_imu_get_gyro_raw_data#
void sl_imu_get_gyro_raw_data (float gvec)
Retrieve the raw gyroscope data from the IMU.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| float | [out] | gvec | Three dimensional raw gyro vector |