Frequently Asked Questions for Matter over Thread#
Demo#
- Why are the - mattertoolcommands not working after all the steps?- Check if the Radio Co-Processor (RCP) image was built and/or flashed correctly to the device. 
- Make sure you see a QR code on the display of the Matter Accessory Device (MAD). 
- Make sure the images being used to flash the Raspberry Pi, RCP and MAD are correct. 
 
- How can I find the IP address of my Raspberry Pi? - First, make sure the Raspberry Pi is connected to a network (ethernet or Wi-Fi). This page has more information: Setting up the Matter Hub (Raspberry Pi) 
- Refer to this page for general questions on finding the Raspberry Pi on your network: Finding your Raspberry Pi 
- For more detailed information, refer to this page: Raspberry Pi Remote Access