Frequently Asked Questions for Matter over Thread#
Demo#
Why are the
mattertoolcommands not working after all the steps?Check if the Radio Co-Processor (RCP) image was built and/or flashed correctly to the device.
Make sure you see a QR code on the display of the Matter Accessory Device (MAD).
Make sure the images being used to flash the Raspberry Pi, RCP and MAD are correct.
How can I find the IP address of my Raspberry Pi?
First, make sure the Raspberry Pi is connected to a network (ethernet or Wi-Fi). This page has more information: Setting up the Matter Hub (Raspberry Pi)
Refer to this page for general questions on finding the Raspberry Pi on your network: Finding your Raspberry Pi
For more detailed information, refer to this page: Raspberry Pi Remote Access