Building in VS Code#
This section covers creating a new sample application from an existing application, which is optional for Building , Flashing and Debugging the target Matter Accessory Devices.
Linux/Mac#
Step 1:#
Use the shortcut (Ctrl + Shift + P) to trigger the command pallet.
Step 2:#
Search for "Run Task" and select the "Copy Sample Application" option.
Step 3:#
On the drop-down menu, select "Copy Sample Application".
Step 4:#
On the next menu select an EFR32 example to copy.
Step 5:#
Select the appropriate target board.


Step 6:#
Provide a name for the sample application target directory in the Matter workspace.
Windows#
Copying a sample application is not supported for Windows at this time.