Matter Software Update with EFR32 Example Applications#
([SIMPLICITY STUDIO] & [GITHUB])
The Over The Air (OTA) Software Update functionality is enabled by default for
all of the EFR32 example applications. Its inclusion in an application is
controlled by the chip_enable_ota_requestor compile flag.
Running the OTA Download Scenario#
For Matter with OpenThread: Bring up the OpenThread Border Router as discussed in Thread Demo Overview and get its operational dataset.
On a Linux or Darwin platform build the chip-tool and the ota-provider-app as follows:
$ scripts/examples/gn_build_example.sh examples/chip-tool out/$ scripts/examples/gn_build_example.sh examples/ota-provider-app/linux out/debug chip_config_network_layer_ble=falseBuild or download the Gecko Bootloader binary. Follow the instructions in Creating the Bootloader for Use in Matter OTA. For the bootloader using the external flash select the "external SPI" bootloader type configured with a single slot of at least 1000 KB. For the bootloader using the internal flash see the Internal Storage Bootloader section below. Pre-built binaries for some configurations are available on the Matter Artifacts page, see README.md for details.
Using the commander tool, upload the bootloader to the device running the application.
Create a bootable image file (using the Lighting application image as an example):
$ commander gbl create chip-efr32-lighting-example.gbl --app chip-efr32-lighting-example.s37Create the Matter OTA file from the bootable image file:
$ ./src/app/ota_image_tool.py create -v 0xFFF1 -p 0x8005 -vn 2 -vs "2.0" -da sha256 chip-efr32-lighting-example.gbl chip-efr32-lighting-example.otaIn a terminal start the Provider app and pass to it the path to the Matter OTA file created in the previous step:
$ rm -r /tmp/chip_* ./out/debug/chip-ota-provider-app -f chip-efr32-lighting-example.otaIn a separate terminal run the chip-tool commands to provision the Provider:
$ ./out/chip-tool pairing onnetwork 1 20202021$ ./out/chip-tool accesscontrol write acl '[{"fabricIndex": 1, "privilege": 5, "authMode": 2, "subjects": [112233], "targets": null}, {"fabricIndex": 1, "privilege": 3, "authMode": 2, "subjects": null, "targets": null}]' 1 0If the application device had been previously commissioned, hold Button 0 for six seconds to factory-reset the device.
In the chip-tool terminal enter:
$ ./out/chip-tool pairing ble-thread 2 hex:<operationalDataset> 20202021 3840
where operationalDataset is obtained from the OpenThread Border Router.
Once the commissioning process completes enter:
$ ./out/chip-tool otasoftwareupdaterequestor announce-ota-provider 1 0 0 0 2 0The application device will connect to the Provider and start the image download. Once the image is downloaded the device will reboot into the downloaded image.
Internal Storage Bootloader#
Internal storage bootloader for Matter OTA software update is supported on MG24 boards only. In this use case both the running image and the downloadable update image must fit on the internal flash at the same time. This in turn requires that both images are built with a reduced feature set, such as disabled logging and Matter shell. The following set of compile flags leaves out all the optional features and results in the minimal image size:
chip_detail_logging=false
chip_automation_logging=false
chip_progress_logging=false
is_debug=false
show_qr_code=false
chip_build_libshell=false
enable_openthread_cli=false
chip_openthread_ftd=trueUsing LZMA compression when building the .gbl file ( passing --compress lzma
parameter to the commander gbl create command) further reduces the downloaded
image size.
When building an internal storage bootloader the two key configuration
parameters are the Slot Start Address and Slot Size in the Bootloader Storage
Slot component. The storage slot must not overlap with the running image and the
NVM section of the flash. In other words, the slot start address must be greater
than the end of the running image address and the sum of the start address and
the slot size must be less than the address of the NVM section. The simplest way
to get the relevant addresses for the running image and NVM is by using the
Silicon Labs Simplicity Commander (Device Info->Main Flash->Flash Map).
The pre-built bootloader binaries are configured with slot start address of 0x080EC000 and slot size of 548864
Managing the Software Version#
In order for the Provider to successfully serve the image to a device during the
OTA Software Update process the Software Version parameter that the .ota file
was built with must be greater than the
CHIP_DEVICE_CONFIG_DEVICE_SOFTWARE_VERSION parameter set in the application's
CHIPProjectConfig.h file. The Software Version parameter is set by the -vn
parameter passed to the ota_image_tool.py create command. For example, if the
application's running image was built with
CHIP_DEVICE_CONFIG_DEVICE_SOFTWARE_VERSION set to 1 and if the .ota file is
built with -vn 2 then the Provider will serve the update image when requested.
In order for the OTA Software Update subsystem to consider an update to be successful and for the NotifyUpdateApplied command to be transmitted the CHIP_DEVICE_CONFIG_DEVICE_SOFTWARE_VERSION in the updated image must exceed the software version of the running image (continuing the above example, the image for the update must be built with CHIP_DEVICE_CONFIG_DEVICE_SOFTWARE_VERSION set to 2).
Managing the Vendor and Product ID#
Starting the ota-provider-app with the --otaImageList command line option allows the user to supply a JSON file specifying the Software Version, Vendor and Product ID that identify the image served by the Provider, see the ota-provider-app for linux in examples directory.
Example provider configuration file:
{ "foo": 1, // ignored by parser
"deviceSoftwareVersionModel":
[
{
"vendorId": 65521, "productId": 32773, "softwareVersion": 1, "softwareVersionString": "1.0.0", "cDVersionNumber": 18, "softwareVersionValid": true, "minApplicableSoftwareVersion": 0, "maxApplicableSoftwareVersion": 100, "otaURL": "chip-efr32-lighting-example.ota"
}
]
}Additional Info#
Developers can find more resources on Silicon Labs Matter Community Page .