Matter Software Artifacts#
This page provides links to pre-built software image "artifacts" that can be used to set up the Matter Demo for the Thread and Wi-Fi use cases.
Matter Hub Raspberry Pi Image#
The Matter Hub image is intended to be flashed onto an SD card for a Raspberry Pi. The Matter Hub Image provides both an Open Thread Border Router and the Matter chip-tool. Note the image is ~10GB in size so depending on your internet connection this download may take some time. Start the Matter Hub Raspberry Pi image download here:
https://www.silabs.com/documents/public/software/SilabsMatterPi_2.1.0-1.1.zip
Radio Co-Processor (RCP) Images#
The Radio Co-Processor firmware is used to turn an EFR into an RCP that can be used with a Raspberry Pi to allow the Raspberry Pi's Open Thread Border Router to access the Thread network. Radio Co-Processor (RCP) images are available in the Assets section of this page:
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
Matter Accessory Device Images#
The Matter Accessory Device Images are used to turn an EFR into a Matter device. These are pre-built binary images for the Matter Demo. Matter Accessory Device Images are located in the Assets section of this page:
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
Matter Bootloader Binaries#
If you are using the OTA functionality and especially if you are using an EFR32MG2x device, you will need to flash a bootloader binary on your device along with the application image. Bootloader binaries for all of the Matter supported devices are available here:
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
RS9116 Firmware#
The RS9116 firmware (rs9116_firmware_files_with_rev.zip) is used to update the RS9116 which can be found in the Assets section of this page:
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
Note: RS9116 chip/module needs to be flashed with proper firmware as mentioned below:
RS916.x.x.x.x.x.rps - This firmware image is valid for RS9116 1.5 revision chip/moduleRS9116.x.x.x.x.x.rps - This firmware image is valid for RS9116 1.4/1.3 revision chip/module
SiWx917 Firmware for SiWx917 NCP#
The SiWx917 firmware(SiWx917NCP_firmware_files.zip) is used to update the SiWx917 NCP which can be found in the Assets section of this page:
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
Note: SiWx917 NCP boards needs to be flashed with proper firmware as mentioned below:
SiWG917-A.1.0.0.0.23.rps - This firmware image is valid for BRD8036A (A0 Expansion v1.0) and BRD8036A (A0 Expansion v1.1) boards
SiWx917 Firmware for SiWx917 SoC#
The SiWx917 firmware (SiWx917SOC_firmware_files.zip) along with WiSeConnect 3 SDK is used to update the SiWx917 SoC which can be found in the Assets section of this page.
https://github.com/SiliconLabs/matter_extension/releases/tag/v2.1.0
Note: SiWx917 SoC boards needs to be flashed with proper firmware as mentioned below:
SiWG917-A.2.9.X.X.X.rps - This firmware image is valid for BRD4325B(A0 dual flash 1.1) and BRD4325B(A0 dual flash 1.2) boardsSiWG917-B.2.9.X.X.X.rps - This firmware image is valid for BRD4325C(B0 common flash v1.2) and BRD4325G(B0 Stacked Flash + External PSRAM v1.2) boards