Matter Custom Part Manufacturing Service (CPMS)#

Tools in the Silicon Labs Matter GitHub cpms folder are used to load mandatory authentication information into Matter devices. For more information on accessing the cpms tools and cloning the Silicon Labs Matter GitHub repository see the documentation located here: Silicon Labs Matter GitHub repo.

Most of the required parameters are stored once during the manufacturing process, and shall not change during the lifetime of the device. During runtime, two interfaces are used to pull the authentication data from permanent storage:

The provisioning script in this folder now supersedes the following tool:

Provisioned Data#

The Commissionable Data includes Serial Number, Vendor Id, Product Id, and the Setup Payload (typicallty displayed in the QR), while the Attestation Credentials includes the Certificate Declaration (CD), the Product Attestation Intermediate (PAI) certificate, and the DAC (Device Attestation Certificate).

During commissioning, Matter devices perform a Password Authenticated Key Exchange using the SPAKE2+ protocol. The SPAKE2+ verifier is pre-calculated using an external tool.

The passcode is used to derive a QR code, typically printed on the label, or displayed by the device itself. The QR code contains the pre-computed setup payload, which allows the commissioner to establish a session with the device. The parameters required to generate and validate the session keys are static and stored in NVM3.

To protect the attestation private-key (used to generate the DAC), the asymmetric key-pair should be generated on-device, using PSA, and the most secure storage location available to the specific part. However, the private-key may be generated externally, and imported using the --dac_key parameter.

The DAC is generated and signed by a Certification Authority (CA), which may reside on a separate host. The modules/signing_server.py script simulates the role of the CA, and uses OpenSSL to to generate and sign the DAC. In a real factory environment, this script is replaced by an actual CA.

Generator Firmware#

The Generator Firmware (GFW) is a baremetal application that runs on the targeted device, and assists with the initial setup of the device. The GFW performs the following tasks:

  • Generates the device key-pair on the most secure location available

  • Returns a CSR (Certificate Signing Request) to the provisioning script. The CSR contains the device public-key, Vendor Id, Product Id, and Serial Number.

  • Calculates the Setup Payload

  • Stores the Commissionable Data into NVM3 (including the Setup Payload)

  • Stores the Attestation Data on the main flash (CD, PAI, DAC)

  • Stores the size and offsets used to store the Attestation Data, along with the KeyId used to generate the private-key

The main source code of the GFW is located under cpms/generator, while the board support is located under cpms/support. Pre-compiled images for the supported chips can be found in cpms/images.

The directory structure is as follows:

  • cpms

    • generator

    • images

    • modules

    • support

      • efr32mg12

      • efr32mg24

Provisioner Script#

The provision.py file is the main script used to load all the required data on the Matter device. This script requires:

sudo pip3 install ecdsa

The Provisioner Script executes the following steps:

  1. Parses and validates the command-line arguments

  2. Obtains the Part Number from the connected device (using Simplicity Commander)

  3. If no SPAKE2+ verifier is provided:    3.1. Generates SPAKE2+ verifier (using the external spake2p tool)

  4. Loads the Generator Firmware into the device (if no GFW path is provided, the Part Number is used to choose the corresponding file from the cpms/images)

  5. Configures the NVM3 based on the flash size of the connected device

  6. If CSR mode is used (--csr):    6.1. Requests a CSR from the device     - The GFW generates the key-pair and CSR, then returns the the CSR to the host script    6.2. Sends the CSR to the Signing Server (cpms/modules/signing_server.py), and retrieves the DAC

  7. Sends CD, PAI, and DAC to the GFW     - The GFW stores CD, PAI, and DAC on the last page of main flash, and updates the offsets and sizes in NVM3

  8. Sends the Commissionable Data to the GFW     - The GFW initializes the flash, generates the Setup Payload, and stores the data into NVM3

  9. If a PFW is provided, writes the PFW into flash using Simplicity Commander

The provisioning script and the GFW communicates through J-Link RTT using the PyLink module.

Arguments#

Arguments

Conformance

Type

Description

-c, --config

optional

string

Path to a JSON configuration file

-j, --jlink

optional ^1

dec/hex

JLink connection string.

-g, --generate

optional

flag

Auto-generate test certificates

-m, --cpms

optional

flag

CPMS mode: When true, only generate the JSON configuration, and exit.

-r, --csr

optional

flag

CSR mode: When true, instructs the GFW to generate the private key, and issue a CSR.

-gf, --gen_fw

optional

dec/hex

Path to the Generator Firmware image.

-pf, --prod_fw

optional

dec/hex

Path to the Production Firmware image.

-v, --vendor_id

optional

dec/hex

Vendor ID. e.g: 65521 or 0xFFF1 (Max 2 bytes).

-V, --vendor_name

optional

string

Vendor name (Max 32 char).

-p, --product_id

optional

dec/hex

Product ID. e.g: 32773 or 0x8005 (Max 2 bytes).

-P, --product_name

optional

string

Product name (Max 32 char).

-pl, --product_label

optional

string

Product label.

-pu, --product_url

optional

string

Product URL.

-pn, --part_number

optional

dec/hex

Device Part Number (Max 32 char).

-hv, --hw_version

optional

dec/hex

The hardware version value (Max 2 bytes).

-hs, --hw_version_str

optional

string

The hardware version string (Max 64 char).

-cf, --commissioning_flow

optional

dec/hex

Commissioning Flow 0=Standard, 1=User Action, 2=Custom.

-rf, --rendezvous_flags

optional

dec/hex

Rendez-vous flag: 1=SoftAP, 2=BLE 4=OnNetwork (Can be combined).

-md, --manufacturing_date

optional

string

Manufacturing date.

-d, --discriminator

optional ^2

dec/hex

BLE pairing discriminator. e.g: 3840 or 0xF00. (12-bit)

-ct, --cert_tool

optional

string

Path to the chip-cert tool. Defaults to ../out/tools/chip-cert

-ki, --key_id

required

dec/hex

Attestation Key ID.

-kp, --key_pass

optional ^3

string

Password for the key file.

-xc, --att_certs

optional ^3

string

Path to the PKCS#12 attestation certificates file.

-ic, --pai_cert

required

string

Path to the PAI certificate.

-dc, --dac_cert

optional ^3

string

Path to the PAI certificate.

-dk, --dac_key

optional ^3

dec/hex

Path to the PAI private-key.

-cd, --certification

required

string

Path to the Certification Declaration (CD) file.

-cn, --common_name

optional ^4

string

Common Name to use in the Device Certificate (DAC) .

-u, --unique_id

optional ^5

hex string

A 128 bits hex string unique id (without 0x).

-sv, --spake2p_verifier

optional

string ^6

Pre-generated SPAKE2+ verifier.

-sp, --spake2p_passcode

required

dec/hex

Session passcode used to generate the SPAKE2+ verifier.

-ss, --spake2p_salt

required

string ^6

Salt used to generate the SPAKE2+ verifier.

-si, --spake2p_iterations

required

dec/hex

Iteration count used to generate the SPAKE2+ verifier.

^1 Use xxxxxxxxx for serial, or xxx.xxx.xxx.xxx[:yyyy] for TCP. ^2 If not provided (or zero), the discriminator is calculated as the last 12 bits of SHA256(serial_number) ^3 If the DAC is provided, its corresponding private-key also must be provided ^4 Required if the DAC is not provided ^5 If not provided, the unique_id is calculated as the first 128 bits of SHA256(serial_number) ^6 Salt and verifier must be provided as base64 string

For the hex type, provide the value with the 0x prefix. For hex string type, do not add the 0x prefix.

The -c/--config argument allows to read all the required parameters from a JSON file. The same validation rules apply both for command line or configuration file, but JSON does not support hexadecimal numbers. Command line arguments override arguments read from a configuration file. For instance, with the configuration cpms.json:

{
    "version": "1.0",
    "matter": {
        "prod_fw": "/git/matter/out/lighting-app/BRD4187C/chip-efr32-lighting-example.s37",
        "vendor_id": 4169,
        "product_id": 32773,
        "discriminator": 3841,
        "attestation": {
            "dac_cert": "temp/certs/dac_cert.pem",
            "dac_key": "temp/certs/dac_key.pem",
            "pai_cert": "temp/certs/pai_cert.pem",
            "certification": "temp/certs/cd.der",
        },
        "spake2p": {
            "passcode": 62034001,
            "salt": "95834coRGvFhCB69IdmJyr5qYIzFgSirw6Ja7g5ySYA",
            "iterations": 15000
        }
    }
}

You may run:

python3 ./provision.py -c cpms.json -d 2748 -p 0x8006 -si 10000

Which will set the connected device with discriminator 2748 (instead of 3841), product ID 32774 (instead of 32773), and use 10000 SPAKE2+ iterations (instead of 15000).

To ease development and testing, the provision.py script provides defaults for most of the parameters. The only arguments that are truly mandatory are vendor_id, and product_id. Test certificates may be auto-generated using the -g flag, provided the chip-cert can be found, either in the default location, or through the --cert-tool argument. For instance, you may run:

python3 ./provision.py -v 0x1049 -p 0x8005 -g

Which will generate the test certificates using chip-cert, and set the device with the following parameters:

{
    "version": "1.0",
    "matter": {
        "generate": true,
        "vendor_id": 65522,
        "product_id": 32773,
        "discriminator": 3840,
        "attestation": {
            "cert_tool": "./out/tools/chip-cert",
            "key_id": 2,
        },
        "spake2p": {
            "verifier": null,
            "passcode": 62034001,
            "salt": "95834coRGvFhCB69IdmJyr5qYIzFgSirw6Ja7g5ySYA=",
            "iterations": 15000
        }
    }
}

For each run, provision.py will generate the file cpms/config/latest.json, containing the arguments used to set up the device. A default configuration with developer settings can be found at cpms/config/develop.json:

python ./provision.py -c config/develop.json

Attestation Files#

The --generate option instructs the provider.py script to generate test attestation files with the given Vendor ID, and Product ID. These files are generated using the chip-cert tool, and stored under the cpms/temp folder.

To generate the certificates manually:

./chip-cert gen-cd -f 1 -V 0xfff1 -p 0x8005 -d 0x0016 -c ZIG20142ZB330003-24 -l 0 -i 0 -n 257 -t 0 -o 0xfff1 -r 0x8005 -C ./credentials/test/certification-declaration/Chip-Test-CD-Signing-Cert.pem -K ./credentials/test/certification-declaration/Chip-Test-CD-Signing-Key.pem -O ./temp/cd.der

./chip-cert gen-att-cert -t a -l 3660 -c "Matter PAA" -V 0xfff1 -o ./temp/paa_cert.pem -O ./temp/paa_key.pem

./chip-cert gen-att-cert -t i -l 3660 -c "Matter PAI" -V 0xfff1 -P 0x8005 -C ./temp/paa_cert.pem -K ./temp/paa_key.pem -o ./temp/pai_cert.pem -O ./temp/pai_key.pem

./chip-cert gen-att-cert -t d -l 3660 -c "Matter DAC" -V 0xfff1 -P 0x8005 -C ./temp/pai_cert.pem -K ./temp/pai_key.pem -o ./temp/dac_cert.pem -O ./temp/dac_key.pem

NOTE: The commissioning fails if the commissioner do not recognize the root certificate (PAA). When using chip-tool, you can use the --paa-trust-store-path to enabled the PAA certificates for testing purposes.

Example#

In Simplicity Studio, add the Matter Device Attestation Credentials component to the project and build it. The resulting s37 file is used as an input to the provision.py script in the next step.

Set up the device with key generation:

python3 ./provision.py -v 0x1049 -p 0x8005 \
    -r -ki 2 -cn "Silabs Device" -ic ./temp/pai_cert.pem -cd ./temp/cd.der \
    -sp 62034001 -ss 95834coRGvFhCB69IdmJyr5qYIzFgSirw6Ja7g5ySYA= -si 15000 \
    -d 0xf01 -j 440266330 -pf chip-efr32-lighting-example.s37

Or, set up the device with imported key:

python3 ./provision.py -v 0x1049 -p 0x8005 \
    -ki 2 -cn "Silabs Device" -dc ./temp/dac_cert.pem  -dk ./temp/dac_key.pem  -ic ./temp/pai_cert.pem -cd ./temp/cd.der \
    -sp 62034001 -ss 95834coRGvFhCB69IdmJyr5qYIzFgSirw6Ja7g5ySYA= -si 15000 \
    -d 0xf01 -j 440266330 -pf chip-efr32-lighting-example.s37

Set up device with PKCS#12 attestation certificates file

python3 ./provision.py -c config/silabs.json -xc certs.p12 -kp cBiqGji1ARHKQ8gv6kiVh1uJQDn/dMXlTXbNOXwjNDE= -cd /certificate.cd -d 0x771

Validation#

If the certificate injection is successful, the commissioning process should complete normally. In order to verify that the new certificates are actually being used, first check the last page of the flash using Commander. The content of the flash must then be compared with the credentials received by the commissioner, which can be done using a debugger.

Flash Dump#

On EFR32MG12, the last page starts at address 0x000FF800. On EFR32MG24, the last page is located at 0x0817E000. These addresses can be found in the memory map of the board's datasheet. For instance, for a MG24 board:

commander readmem --range 0x0817E000:+1536 --serialno 440266330`

The output should look something like:

commander readmem --range 0x0817E000:+1536 --serialno 440266330
Reading 1536 bytes from 0x0817e000...
{address:  0  1  2  3  4  5  6  7  8  9  A  B  C  D  E  F}
000ff800: 30 82 01 D8 30 82 01 7F A0 03 02 01 02 02 04 07
000ff810: 5B CD 15 30 0A 06 08 2A 86 48 CE 3D 04 03 02 30
...
000ff9c0: 2B BA 15 32 2F 4C 69 F2 38 48 D2 BC 62 2A 47 FB
000ff9d0: 3F F7 28 8A 7C 90 75 72 58 84 96 E7 00 00 00 00
000ff9e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ff9f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ffa00: 30 82 01 C8 30 82 01 6E A0 03 02 01 02 02 08 79
000ffa10: 6E 32 5A FA 5B D1 F8 30 0A 06 08 2A 86 48 CE 3D
...
000ffbb0: FD 92 D1 EB 59 95 D8 38 DE 5D 80 E3 05 65 24 4A
000ffbc0: 62 FD 9F E9 D8 00 FA CD 0F 32 7C C9 00 00 00 00
000ffbd0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ffbe0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ffbf0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ffc00: 30 81 EF 06 09 2A 86 48 86 F7 0D 01 07 02 A0 81
000ffc10: E1 30 81 DE 02 01 03 31 0D 30 0B 06 09 60 86 48
...
000ffce0: 28 41 FD B8 28 CD 19 F2 BB DB A0 0F 33 B2 21 D3
000ffcf0: 33 CE 00 00 00 00 00 00 00 00 00 00 00 00 00 00
000ffd00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

On this example, the DAC is located at address 0817e000 (offset 0), and has 476 octets:

0817e000: 30 82 01 D9 30 82 01 7F A0 03 02 01 02 02 04 07
0817e010: 5B CD 15 30 0A 06 08 2A 86 48 CE 3D 04 03 02 30
...
0817e1c0: 2E 4F 10 20 38 BA A6 B5 F6 A4 77 7A 19 91 23 79
0817e1d0: 2F A0 FF AF F5 5C A1 59 98 08 C7 BC 5F 00 00 00

This should match the contents of the DER-formatted DAC certificate, which is stored by the setup script as ./temp/dac.der :

$ xxd ./temp/dac.der
00000000: 3082 01d8 3082 017f a003 0201 0202 0407  0...0...........
00000010: 5bcd 1530 0a06 082a 8648 ce3d 0403 0230  [..0...*.H.=...0
...
000001c0: 2bba 1532 2f4c 69f2 3848 d2bc 622a 47fb  +..2/Li.8H..b*G.
000001d0: 3ff7 288a 7c90 7572 5884 96e7            ?.(.|.urX...


The PAI certificate is located at address 0x0817e200 (offset 512), and
has 460 octets:
0817e200: 30 82 01 C8 30 82 01 6E A0 03 02 01 02 02 08 79
0817e210: 6E 32 5A FA 5B D1 F8 30 0A 06 08 2A 86 48 CE 3D
...
0817e3b0: FD 92 D1 EB 59 95 D8 38 DE 5D 80 E3 05 65 24 4A
0817e3c0: 62 FD 9F E9 D8 00 FA CD 0F 32 7C C9 00 00 00 00

This should match the contents of the DER-formatted PAI certificate, which is stored by the setup script as ./temp/pai_cert.der :

$ xxd ./temp/pai_cert.der
00000000: 3082 01c8 3082 016e a003 0201 0202 0879  0...0..n.......y
00000010: 6e32 5afa 5bd1 f830 0a06 082a 8648 ce3d  n2Z.[..0...*.H.=
...
000001b0: fd92 d1eb 5995 d838 de5d 80e3 0565 244a  ....Y..8.]...e$J
000001c0: 62fd 9fe9 d800 facd 0f32 7cc9            b........2|.

Finally, on this example the CD is located at address 0817e400 (offset 1024), and contains 541 octets:

0817e400: 30 81 EF 06 09 2A 86 48 86 F7 0D 01 07 02 A0 81
0817e410: E1 30 81 DE 02 01 03 31 0D 30 0B 06 09 60 86 48
...
0817e4d0: 02 20 38 B9 9C 73 B2 30 92 D7 A2 92 47 30 14 F7
0817e4e0: 28 41 FD B8 28 CD 19 F2 BB DB A0 0F 33 B2 21 D3
0817e4f0: 33 CE 00 00 00 00 00 00 00 00 00 00 00 00 00 00

The CD is a binary file, and is neither modified, nor validated by the setup script. It is simply stored in flash after the DAC:

$ xxd cd.der
00000000: 3081 ef06 092a 8648 86f7 0d01 0702 a081  0....*.H........
00000010: e130 81de 0201 0331 0d30 0b06 0960 8648  .0.....1.0...`.H
...
000000e0: 2841 fdb8 28cd 19f2 bbdb a00f 33b2 21d3  (A..(.......3.!.
000000f0: 33ce                                     3.

The 0xff octets between the files and at the end of the flash are unmodified sections of the flash storage.

Device Terminal#

Logs have beed added to the SilabsDeviceAttestationCreds, to help verifying if the Attestation files are loaded correctly. The size and first eight bytes of CD, PAI, and DAC are printed, and must match the contents of cd.der, pai_cert.der, and dac.der, respectively:

...
[00:00:05.109][info  ][ZCL] OpCreds: Certificate Chain request received for PAI
[00:00:05.109][info  ][DL] GetProductAttestationIntermediateCert, addr:0xffa00, size:460
[00:00:05.110][detail][ZCL] 0x30, 0x82, 0x01, 0xc8, 0x30, 0x82, 0x01, 0x6e,
...
[00:00:05.401][info  ][ZCL] OpCreds: Certificate Chain request received for DAC
[00:00:05.402][info  ][DL] GetDeviceAttestationCert, addr:0xff800, size:477
[00:00:05.402][detail][ZCL] 0x30, 0x82, 0x01, 0xd8, 0x30, 0x82, 0x01, 0x7f,
...

[00:00:05.694][info  ][ZCL] OpCreds: Received an AttestationRequest command
[00:00:05.695][info  ][DL] GetCertificationDeclaration, addr:0xffc00, size:242
[00:00:05.695][detail][ZCL] 0x30, 0x81, 0xef, 0x06, 0x09, 0x2a, 0x86, 0x48,
...

Board Support#

Pre-compiled images of the Generator Firmware can be found under cpms/images. The source code of these images is found under cpms/support. A single image is provided for all EFR32MG12 parts, and another one for the EFR32MG24 family. To copy with the different flash sizes, the provision.py script reads the device information using commander, and send it to the GFW, which configures the NVM3 during the initialization step.