Set Up MQTT Explorer#
Download and install the MQTT Explorer from https://mqtt-explorer.com/ Setting up MQTT Explorer for testing.


Connecting to MQTT Server#
Connecting to AWS#
Host : Your Host name (examples: a2m21kovu9tcsh-ats.iot.ap-southeast-1.amazonaws.com)
Port : 8883
Make sure you enable
Validate Certificate and EncryptionClick on the
Advanced Settings


Add application specific topics as shown below - For Lighting app, topic to be added (light/) - For onoff plug app, topic to be added (light/) - For Lock app, topic to be added (lock/) - For thermostat app, below topics to be added - LocalTemperature/ - OccupiedCoolingSetpoint/* - OccupiedHeatingSetpoint/* - thermostat/* - For Windows app, below topics to be added - lift/* - tilt/*
MQTT Client ID depends on the certificate set that you will use.
Add the Certificate, following step 7 in AWS installation


Once the above steps are done, try connecting to AWS.


Connecting to Mosquitto Connection#
Host : Your Mosquitto ip address
Port : 8883
Make sure you enable Validate Certificate and Encryption
Click on the
Advanced Settings


Add application specific topics as shown below
For Lighting app, topic to be added (light/*)
For onoff plug app, topic to be added (light/*)
For Lock app, topic to be added (lock/*)
For thermostat app, below topics to be added
LocalTemperature/*
OccupiedCoolingSetpoint/*
OccupiedHeatingSetpoint/*
thermostat/*
For Windows app, below topics to be added
lift/*
tilt/*
MQTT Client ID depends on the certificate set that you will use.
Add the Certificate, following step 5 in openssl certificate create