Running the Matter Demo over Wi-Fi#
Follow the procedure below to run Matter demo over Wi-Fi.
Flashing the Connectivity Firmware#
To flash the connectivity firmware on an NCP device, refer to the following guide: Upgrading Connectivity Firmware for NCP Devices.
To flash the connectivity firmware on a SiWx917 SoC, refer to the following guide Upgrading Connectivity Firmware for SoC Devices.
Flashing the Bootloader Binary#
The bootloader binary is supported on EFR32 boards only and it can be flashed using the Simplicity Commander software or Simplicity Studio.
To Flash the Bootloader Binary for EFR32 Board, refer to the following guide: Flashing Bootloader Binaries on EFR32 Devices.
Building and Flashing the Matter Application using Simplicity Studio#
To build and flash an application for the EFR32, refer to EFR32 Building and Flashing Application.
To build and flash an application for SiWx917 SoC, refer to SiWx917 SOC Building and Flashing Application.
Flashing the Matter Pre-Built Binaries Using Simplicity Commander#
To flash the application for EFR32 Board using Simplicity Commander, refer to Flash EFR32 Binaries using Simplicity Commander.
Note: For EFR32, you must use the .s37 format file only.
To flash the application for the SiWx917 SoC Board using Simplicity Commander, refer to Flash SiWx917 SoC Matter Pre-Built Binaries.
Note: For SiWx917 SoC, use the .rps format file only.
Setting up the Raspberry Pi#
To set up the Raspberry Pi, refer to Setting up the chip-tool on Raspberry PI.