Matter Provisioning#
Tools in the Silicon Labs Matter GitHub provision folder are used to load mandatory authentication information into Matter devices. For more information on accessing the provision tools and cloning the Silicon Labs Matter GitHub repository, see the documentation located here: Silicon Labs Matter GitHub repo.
Most of the required parameters are stored once during the manufacturing process, and shall not change during the lifetime of the device. During runtime, two interfaces are used to pull the authentication data from permanent storage:
CommissionableDataProvider, implemented as BLEManagerImpl
DeviceAttestationCredsProvider, implemented as SilabsDeviceAttestationCreds
The provisioning script in this folder now supersedes the following tool:
Provisioned Data#
The Commissionable Data includes Serial Number, Vendor Id, Product Id, and the Setup Payload (typically displayed in the QR), while the Attestation Credentials includes the Certificate Declaration (CD), the Product Attestation Intermediate (PAI) certificate, and the DAC (Device Attestation Certificate).
During commissioning, Matter devices perform a Password Authenticated Key Exchange using the SPAKE2+ protocol. The SPAKE2+ verifier is pre-calculated using an external tool.
The passcode is used to derive a QR code, typically printed on the label, or displayed by the device itself. The QR code contains the pre-computed setup payload, which allows the commissioner to establish a session with the device. The parameters required to generate and validate the session keys are static and stored in NVM3.
To protect the attestation private-key (used to generate the DAC), the asymmetric key-pair should be generated on-device, using PSA, and the most secure storage location available to the specific part. However, the private-key may be generated externally, and imported using the --dac_key parameter.
The DAC is generated and signed by a Certification Authority (CA), which may reside on a separate host. The modules/signing_server.py script simulates the role of the CA, and uses OpenSSL to to generate and sign the DAC. In a real factory environment, this script is replaced by an actual CA.
Generator Firmware#
The Generator Firmware (GFW) is a baremetal application that runs on the targeted device, and assists with the initial setup of the device. The GFW performs the following tasks:
Generates the device key-pair on the most secure location available
Returns a CSR (Certificate Signing Request) to the provisioning script. The CSR contains the device public-key, Vendor Id, Product Id, and Serial Number.
Calculates the Setup Payload
Stores the Commissionable Data into NVM3 (including the Setup Payload)
Stores the Attestation Data on the main flash (CD, PAI, DAC)
Stores the size and offsets used to store the Attestation Data, along with the KeyId used to generate the private-key
The main source code of the GFW is located under provision/generator, while the board support is located under provision/support. Pre-compiled images for the supported chips can be found in provision/images.
The directory structure is as follows:
provision
generator
images
modules
support
efr32mg12
efr32mg24
Provisioner Script#
The provision.py file is the main script used to load all the required data on the Matter device. This script requires:
sudo pip3 install ecdsa
The Provisioner script executes the following steps:
Parses and validates the command-line arguments.
Obtains the Part Number from the connected device (using Simplicity Commander).
If no SPAKE2+ verifier is provided:
Generates SPAKE2+ verifier (using the external
spake2ptool).
Loads the Generator Firmware into the device (if no GFW path is provided, the Part Number is used to choose the corresponding file from the
provision/images).Configures the NVM3 based on the flash size of the connected device.
If CSR mode is used (--csr):
Requests a CSR from the device. The GFW generates the key-pair and CSR, then returns the the CSR to the host script.
Sends the CSR to the Signing Server (
provision/modules/signing_server.py), and retrieves the DAC.
Sends CD, PAI, and DAC to the GFW.
The GFW stores CD, PAI, and DAC on the last page of main flash, and updates the offsets and sizes in NVM3
Sends the Commissionable Data to the GFW.
The GFW initializes the flash, generates the Setup Payload, and stores the data into NVM3
If a PFW is provided, writes the PFW into flash using Simplicity Commander.
The provisioning script and the GFW communicates through J-Link RTT using the PyLink module.
Arguments#
Arguments | Conformance | Type | Description |
|---|---|---|---|
-c, --config | optional | string | Path to a JSON configuration file. |
-j, --jlink | optional ^1 | dec/hex | JLink connection string. |
-l, --pylink_lib | optional | string | Path to the PyLink library. |
-g, --generate | optional | flag | Auto-generate test certificates. |
-m, --stop | optional | flag | Stop mode: When true, only generate the JSON configuration, and exit. |
-r, --csr | optional | flag | CSR mode: When true, instructs the GFW to generate the private key, and issue a CSR. |
-gf, --gen_fw | optional | dec/hex | Path to the Generator Firmware image. |
-pf, --prod_fw | optional | dec/hex | Path to the Production Firmware image. |
-v, --vendor_id | optional | dec/hex | Vendor ID. e.g: 65521 or 0xFFF1 (Max 2 bytes). |
-V, --vendor_name | optional | string | Vendor name (Max 32 char). |
-p, --product_id | optional | dec/hex | Product ID. e.g: 32773 or 0x8005 (Max 2 bytes). |
-P, --product_name | optional | string | Product name (Max 32 char). |
-pl, --product_label | optional | string | Product label. |
-pu, --product_url | optional | string | Product URL. |
-pn, --part_number | optional | dec/hex | Device Part Number (Max 32 char). |
-hv, --hw_version | optional | dec/hex | The hardware version value (Max 2 bytes). |
-hs, --hw_version_str | optional | string | The hardware version string (Max 64 char). |
-cf, --commissioning_flow | optional | dec/hex | Commissioning Flow 0=Standard, 1=User Action, 2=Custom. |
-rf, --rendezvous_flags | optional | dec/hex | Rendez-vous flag: 1=SoftAP, 2=BLE 4=OnNetwork (Can be combined). |
-md, --manufacturing_date | optional | string | Manufacturing date. |
-d, --discriminator | optional ^2 | dec/hex | BLE pairing discriminator. e.g: 3840 or 0xF00. (12-bit). |
-ct, --cert_tool | optional | string | Path to the chip-cert tool. Defaults to |
-ki, --key_id | required | dec/hex | Attestation Key ID. |
-kp, --key_pass | optional ^3 | string | Password for the key file. |
-xc, --att_certs | optional ^3 | string | Path to the PKCS#12 attestation certificates file. |
-ic, --pai_cert | required | string | Path to the PAI certificate. |
-dc, --dac_cert | optional ^3 | string | Path to the PAI certificate. |
-dk, --dac_key | optional ^3 | dec/hex | Path to the PAI private-key. |
-cd, --certification | required | string | Path to the Certification Declaration (CD) file. |
-cn, --common_name | optional ^4 | string | Common Name to use in the Device Certificate (DAC). |
-u, --unique_id | optional ^5 | hex string | A 128 bits hex string unique id (without 0x). |
-sv, --spake2p_verifier | optional | string ^6 | Pre-generated SPAKE2+ verifier. |
-sp, --spake2p_passcode | required | dec/hex | Session passcode used to generate the SPAKE2+ verifier. |
-ss, --spake2p_salt | required | string ^6 | Salt used to generate the SPAKE2+ verifier. |
-si, --spake2p_iterations | required | dec/hex | Iteration count used to generate the SPAKE2+ verifier. |