Google Ecosystem Setup and Demo Execution#
Hardware Requirements#
For the hardware required for the Google Nest Hub Ecosystem, refer to the Ecosystem overview Prerequisites section.
Software Requirements#
Google Account
Google Home App
Set Up Google Home and Android Smartphone#
Prerequisites for Google Setup#
To run the Google Ecosystem demo, you need both Google and a Matter device. You also need a Google Nest Hub 2nd Generation and an Android phone (at least a Pixel 5 is recommended) that can run at least Android 8 (8.1, API Level 27) or newer and has Bluetooth LE capability.
Set Up the Android Phone#
Follow these instructions to set up the Android phone with the necessary applications:
Follow the in-app steps.
NOTE: Currently SiWx917 SoC only supports 2.4GHz channels so ensure that the phone and hub are connected to the 2.4GHz WiFi SSID.
Matter Integration Setup in the Developer Console#
You have now completed setting up the following:
Your home in the Google home app in your Android smartphone
A device running the Matter application e.g. lighting, light-switch, lock.
Having finished the above, the only step left to have your setup ready is to open a QR code webpage for the light device type in your PC. A QR Code link will be present in Device configuration section of logs. Copy the link and paste it in google chrome so you will be able to QR Code.


Matter Demo Execution using Google Home#
Commission Matter Device through Google Home App#
Refer to Getting Started Overview Guide for setting up a Silicon Labs Matter Accessory Device.
Connect board to a computer.
For Wi-Fi NCP Mode Boards, see Connect EFR32 Board to Computer.
For Wi-Fi SOC Mode Boards, see Connect SiWx917 SOC to Computer.
Flash the bootloader binary for your device along with the application (for example, lighting, lock, thermostat, window covering, or light-switch) using Simplicity Commander.
Open the Google Home app on your phone.
Click Devices Section and tap Add.


On the Set up a device screen, tap New device.


NOTE: If the device is running a development version of the application, a prompt will appear stating that "Uncertified device". Proceed to set up the device anyway.
On the Choose a home screen, select your home and tap Next.


The Google Home App searches for a nearby Matter device.


If the device is found, tap the application that you flashed on the device, such as Light or Lock.
If the device is not found, tap Matter-enabled device.


Once the Google Home app has found the device, it will ask you to scan its QR code.
Google Home app asks if you want to connect this device to your Google account. Tap Agree.


The Google Home app now starts to commission the device with Bluetooth LE.


Once you see the Device connected message, tap Done.


The Google Home App now asks you to select a room where you want to keep the Application. You can select any room from the list and tap Next.


At the prompt to create a unique name for the application (For Example: Light, Lock), create any name to identify the application and tap Next.


You will now see your device (for example, Light) shown as being connected to your Google account and added to your selected room at Step 15.


Control the Light via Google Home App#
In the Google Home app, you will now be able to tap your light to turn it ON and OFF.
You can control the light by giving a voice command (for example, 'Ok Google! Turn ON Light') and through the app user interface.
You will see the LED1 on your WSTK board turned on or off depending on the command you enter.
Deleting Matter Application from Google Home#
Press and hold Matter Application for a detailed view.
Tap Setting on the top right corner.
Select the Remove device option.
At Unlink all Matter apps & services from device, select Unlink.