Using the Mattertool (chip-tool)#
The following commands show how to commission a 917 SoC Matter End Device (Matter Accessory Device), and then send the on/off commands with the mattertool automated script. The mattertool script provides an interface into various chip-tool commands used to create and interact with a Matter network.
Prerequisites#
Download the raspi image and flash the image onto pi using with default 'ubuntu' username and enable ssh in the options.
https://www.silabs.com/documents/public/software/SilabsMatterPi_2.4.0-1.4-extension.zip
Erase 917 SoC (brd4338a) and Flash the lighting app on 917 SoC and flash the connectivity firmware image.
command for commission using mattertool :
mattertool bleWifi -s <SSID> -p <passcode>Basic Mattertool Commands#
Context | Command | Usage |
|---|---|---|
|
| Starts commissioning of a Matter Accessory Device using the chip-tool |
|
| Commission a Matter end device which is already in the IPv6 local network |
|
| using it's pairing code |
|
| Open a commissioning window for a Matter end device |
|
| so that it can join another fabric |
|
| Sends the on command to the Matter Accessory Device using the chip-tool |
|
| Sends the off command to the Matter Accessory Device using the chip-tool |
|
| Control the OnOff cluster of a specific Endpoint of a specific device |
You can also use the full chip-tool command set (still using mattertool):
$ mattertool levelcontrol read current-level 106 1Command | Description |
|---|---|
help | Prints help options |
bleWifi | For Matter Bluetooth LE Wi-FI commissioning with 917 SoC device |
buildCT | Clean build of the chip-tool |
cleanVars | Erase every Set variable used in the script. They will be set back to default or randomized value |
off | Turn off the Light on the already-commissioned 917 SoC device |
on | Turn on the Light on the already-commissioned 917 SoC device |
toggle | Toggle the Light on the already-commissioned 917 SoC device |
parsePayload | Parse the given Payload (QrCode string) |
rebuildCT | Rebuild the chip-tool |
vars | Print the Variables in use by the script |
Some options/arguments can be added to the command to update the values of the variables used by the script.
Available commands:
Command | Description |
|---|---|
-h, --help | Prints help options |
-n, --nodeId DIGIT | Specify the Nodeid you are trying to reach |
-e, --endpoint DIGIT | Specify an endpoint for the desired cluster |
-s, --ssid STRING | Wi-Fi AP SSID that the end devices need to connect to |
-p, --password STRING | Wi-Fi AP password |
These configurations are held until overwritten, cleared with cleanVars or when Raspberry Pi reboots.
Active variables used by mattertool:
Variable | Value |
|---|---|
MATTER_ROOT | /home/ubuntu/connectedhomeip |
CHIPTOOL_PATH | /home/ubuntu/connectedhomeip/out/standalone/chip-tool |
NODE_ID | 31354 |
PINCODE | 20202021 |
DISCRIMINATOR | 3840 |
SSID | <your_SSID> |
lastNodeId | 0 |
You can preset them with export X=Y before running the script or use some available options to change some of them.
In most cases, MATTER_ROOT, CHIPTOOL_PATH, PINCODE, and DISCRIMINATOR should remain at the default set value.
For commissioning commands ( bleWifi), NODE_ID will be randomized if it is the same as the last pairing.
Scripts Alias#
The commands presented above are linked to scripts. You can edit .bashrc and rename the following alias to your liking.
$ alias mattertool=‘source $HOME/scripts/matterTool.sh’