Build Procedure For Wi-Fi Direct Internet Connectivity (DIC)#
The following components are common for all apps and should be modified in the corresponding app specific .slcp file.
How to Add the DIC Component#
To add the DIC component, modify the corresponding app specific .slcp file.
- id: matter_dic
from: matterHow to Add the DIC AWS OTA Component#
To add the DIC AWS OTA component, modify the corresponding app specific .slcp file.
- id: aws_ota_wifi_dic
from: matterNote: Building with aws_ota_wifi_dic component enables matter_dic component by default.
Building DIC Application#
After modification in the .slcp Project file as above step, refresh the matter-extension in Simplicity Studio.
Select Preferences in the Launcher tab.


Expand Simplicity Studio section and click on SDKs Tab.


Expand Simplicity SDK and click the Refresh button from side menu.


Build the DIC application using Simplicity Studio
Compile Using New/Different Certificates#
Two devices should not use the same
DIC_CLIENT_ID. To use a different Client ID for your second connection, do the following:If using AWS, change the following file
matter_extension/examples/platform/silabs/DIC/matter_abs_interface/src/dic_nvm_cert.cppunder#if USE_AWS.Use
DIC_SERVER_HOSTname with your Server host name.For Example: a2m21kovu9tcsh-ats.iot.ap-southeast-1.amazonaws.com
Use AWS CA certificate as ca_certificate, device_certificate and device_key with your device cert and device key.
Use
DIC_CLIENT_IDmacro value with your Client ID inmatter_extension/examples/platform/silabs/DIC/matter_abs_interface/inc/dic_config.hThe preferred certificate type to use in the application is ECDSA.
If using mosquitto, change the following file
matter_extension/examples/platform/silabs/DIC/matter_abs_interface/src/dic_nvm_cert.cppenableUSE_MOSQUITTOand disableUSE_AWS.Under
#if USE_MOSQUITTOUse
DIC_SERVER_HOSTname with your Server host name where Mosquitto Broker is running.Use OpenSSL CA certificate as ca_certificate, device_certificate and device_key.
DIC_CLIENT_IDis not required here butDIC_CLIENT_USERandDIC_CLIENT_PASSinmatter_extension/examples/platform/silabs/DIC/matter_abs_interface/inc/dic_config.hneeds to be updated as per your Mosquitto password file.The preferred certificate type to use in the application is ECDSA.