Edit

Using the Mattertool (chip-tool)#

The following commands show how to start a new Thread network from the local OTBR, commission an EFR32 Matter End Device (Matter Accessory Device), and then send the on/off commands with the mattertool automated script. The mattertool script provides an interface into various chip-tool and otbr commands used to create and interact with a Matter network.

Basic Mattertool Commands#

Context

Command

Usage

Initialization

mattertool startThread

Start a Thread network on the OTBR

Commissioning

mattertool bleThread

Start Commissioning a Matter Device using the chip-tool

Commissioning

mattertool pairing ble-thread <node_id> <Thread dataset> <pincode> <discriminator>

Commission a Matter Device with provided pincode and discriminator

Commissioning

mattertool pairing code <node_id> <pairing code>

Commission a Matter Device on the IPv6 local network with pairing code

Multi-fabric

mattertool pairing open-commissioning-window <node_id> <option> <window_timeout> <iteration> <discriminator>

Open a commissioning window for a Matter end device

Matter Light

mattertool on

Sends the on command to the Matter Device using the chip-tool

Matter Light

mattertool off

Sends the off command to the Matter Device using the chip-tool

Matter Light

mattertool onoff <action> <node_id> <endpoint_id>

Control the OnOff cluster of a specific Endpoint of a specific device

Matter Door Lock

mattertool doorlock set-user <OperationType> <UserIndex> <UserName> <UserUniqueId> <UserStatus> <UserType> <CredentialRule> <node_id> <endpoint_id> --timedInteractionTimeoutMs <timeout value>

Set a user for a Matter Lock

Matter Door Lock

mattertool doorlock set-credential <OperationType> <Credential> <CredentialData> <UserIndex> <UserStatus> <UserType> <node_id> <endpoint_id> --timedInteractionTimeoutMs <timeout value>

Set credential for a specific user of a Matter Lock

Matter Door Lock

mattertool doorlock unlock-door <node_id> <endpoint_id> --timedInteractionTimeoutMs <timeout value>

Unlock a Matter Lock

Matter Door Lock

mattertool doorlock lock-door <node-id/group-id> --timedInteractionTimeoutMs <timeout value>

Lock a Matter Lock

Device interaction

mattertool levelcontrol move-to-level <desired_level> 0 1 1 <node_id> <endpoint_id>

Set the brightness level for a Matter dimmable light

Matter RGB Light

mattertool colorcontrol move-to-saturation <desired_saturation> 0 1 1 <node_id> <endpoint_id>

Set the saturation level for a Matter RGB light

Matter RGB Light

mattertool colorcontrol move-to-hue <desired_hue> 0 0 1 1 <node_id> <endpoint_id>

Set the hue level for a Matter RGB light

Matter Thermostat

mattertool thermostat read local-temperature <node_id> <endpoint_id>

Read the local temperature from a Matter thermostat

Matter Window Cover

mattertool windowcovering go-to-lift-value <LiftValue> <node_id> <endpoint_id>

Move the windows cover to a specific lift value

Matter Window Cover

mattertool windowcovering up-or-open <node_id> <endpoint_id>

Open the windows cover

Matter Occupancy Sensor

mattertool occupancysensing read occupancy <node_id> <endpoint_id>

Read the occupancy status of a Matter occupancy sensor

You can also use the full chip-tool command set (still using mattertool):

$ mattertool levelcontrol read current-level 106 1

Advanced Information on the Matter Hub#

Image Tree#

Open Thread Border Router (OTBR)#

For information on what commits to use for the OTBR and RCP, see the Matter Repositories and Commit Hashes page.

The pre-installed OTBR is configured for the infrastructure interface eth0.

Bash script to modify, reinstall, or update the OTBR:

$ otbrsetup

This bash script centralizes and simplifies the local OTBR installation.

Available commands:

Command

Description

-h, --help

Prints help options

-if, --interface <eth0|wlan0>

Select infrastructure interface. Default eth0

-i, --install

Bootstrap, set up and install the OTBR. Usually for a new installation

-s, --setup

Runs the OTBR setup only, use this to change the configured infrastructure interface (use in combination with -if wlan0 for Wi-Fi)

-u, --update

Update the OTBR installation after the repo is updated

Usage#

Change infrastructure to wlan0: $ otbrsetup -if wlan0 -s

Rerun full install for eth0 interface: $ otbrsetup -i

Upgrading the OpenThread Border Router (OTBR)#

Change OTBR commit reference/version:

$ cd /home/ubuntu/ot-br-posix
$ git fetch
$ git checkout <SHA>
$ otbrsetup -u

Upgrading the Matter Chip-Tool#

For more information on the commit hashes used for this demo, consult the following page: Matter Repositories and Commit Hashes.

To change the chip-tool commit reference/version, follow these steps:

$ cd /home/ubuntu/connectedhomeip
$ git fetch
$ git checkout <SHA>
$ mattertool buildCT

The mattertool script centralizes and simplifies the use of chip-tool and starting a clean thread network.

Available commands:

Command

Description

help

Prints help options

startThread

Start a new thread network and store the operational thread dataset for the commissioning purpose (bleThread)

bleThread

For Matter Bluetooth LE thread commissioning with an EFR32 device

bleWifi

For Matter Bluetooth LE Wi-FI commissioning with an EFR32 device

buildCT

Clean build of the chip-tool

cleanVars

Erase every Set variable used in the script. They will be set back to default or randomized value

off

Turn off the Light on the already-commissioned EFR32 device

on

Turn on the Light on the already-commissioned EFR32 device

toggle

Toggle the Light on the already-commissioned EFR32 device

parsePayload

Parse the given Payload (QrCode string)

rebuildCT

Rebuild the chip-tool

vars

Print the Variables in use by the script

Some options/arguments can be added to the command to update the values of the variables used by the script.

Available commands:

Command

Description

-h, --help

Prints help options

-n, --nodeId DIGIT

Specify the Nodeid you are trying to reach

-e, --endpoint DIGIT

Specify an endpoint for the desired cluster

-d, --dataset HEX_STRING

Thread Operation Dataset to be provisioned

-s, --ssid STRING

Wi-Fi AP SSID that the end devices need to connect to

-p, --password STRING

Wi-Fi AP password

These configurations are held until overwritten, cleared with cleanVars, or when Raspberry Pi reboots.

Active variables used by mattertool:

Variable

Value

MATTER_ROOT

/home/ubuntu/connectedhomeip

CHIPTOOL_PATH

/home/ubuntu/connectedhomeip/out/standalone/chip-tool

NODE_ID

31354

THREAD_DATA_SET

<the_value_you_get>

PINCODE

20202021

DISCRIMINATOR

3840

SSID

<your_SSID>

lastNodeId

0

You can preset them with export X=Y before running the script or use some available options to change some of them.

In most cases, MATTER_ROOT, CHIPTOOL_PATH, PINCODE, and DISCRIMINATOR should remain at the default set value.

For commissioning commands (bleThread, bleWifi), NODE_ID will be randomized if it is the same as the last pairing.

When the startThread command is used, THREAD_DATA_SET will be assigned with the right operation dataset for the created Thread Network.

Scripts Alias#

The commands presented above are linked to scripts. You can edit .bashrc and rename the following alias.

$ alias mattertool=‘source $HOME/scripts/matterTool.sh’
$ alias otbrsetup=‘source $HOME/scripts/setupOTBR.sh'