Edit

Optimizing Memory Usage#

This page provides information on optimizing memory usage for Silicon Labs devices.

How to Optimize Memory#

To optimize an application's memory footprint, check the following:

  1. Analyze and reduce stack usage of the application wherever possible.

  2. Disable any included debug modules.

  3. Turn off unused peripherals, features, and functions.

Disabling Debug Logging#

Memory can be optimized by disabling debug logs. The matter_no_debug component disables the following from the project.

  • Disables Silabs specific logging used in Matter

  • Disables Hard Fault logs

  • Keeps Log Level to None

To add matter_no_debug Component, modify the corresponding app-specific .slcp project file.

 - id: matter_no_debug  
   from: matter