Edit

Running the Matter Demo over Wi-Fi#

Follow the procedure below to run the Matter demo over Wi-Fi.

Flashing the Bootloader Binary#

Note: Flashing the bootloader binaries is only required for NCP devices (MG24); it is not applicable to the SiWx917 SoC.

  • The bootloader binary is supported on EFR32 boards only and it can be flashed using the Simplicity Commander software or Simplicity Studio.

  • To Flash the Bootloader Binary for EFR32 Board, refer to the following guide: Flashing Bootloader Binaries on EFR32 Devices.

Flashing the Connectivity Firmware#

Building and Flashing the Matter Application using Simplicity Studio#

Flashing the Matter Pre-Built Binaries Using Simplicity Commander#

Setting up the Raspberry Pi#

To set up the Raspberry Pi, refer to Setting up the chip-tool on Raspberry PI.

Next Steps#