Using the Pre-Built Raspberry Pi "Matter Hub" Image#
When using a Raspberry Pi as a controller in your Matter network, you have two options.
Building the Raspberry Pi Environment "from scratch" using a Raspberry Pi 4.
Using the Silicon Labs Pre-Built Raspberry Pi image available on the Matter Artifacts page page.
Building Environment using Raspberry Pi 4#
Flash the Ubuntu OS Onto the SD Card#
Insert the flashed SD card (directly or using a card reader) into the laptop/PC that will run the Raspberry Pi Imager tool.
Launch the Raspberry Pi 4 Imager.
Flash the Pi image using any one of the following procedures:
Click Choose OS > Other General-purpose OS > Ubuntu >Ubuntu xx.xx 64-bit server OS.
Note: Flash the latest version of Ubuntu Server (64-bit server OS for arm64 architecture).
Download the Matter Hub Raspberry Pi Image provided on the Matter Artifacts page, then click Choose OS > Use custom, and then select the Matter Hub Raspberry Pi Image that you downloaded.
Click Storage and select the SD card detect.
This Raspberry Pi 4's console can be accessed in multiple ways. In this guide, Raspberry Pi 4 is being accessed using PuTTY.
Enter the details like User name, Password, SSID, and its password to connect to the network. Click Save.
Click Write and then Yes when you are asked for permission to erase data on the SD card. It will then start flashing the OS onto the SD card.
When it is done, click Continue.
Remove the SD card from the reader and insert it into the Raspberry Pi as shown below:


On powering up the board, the red and green lights should start blinking.
Start Using the Raspberry Pi#
Power-up the RPi4B. Once it is booted up, check the Raspberry Pi's IP address. Refer to Finding Raspberry Pi IP address in the Resources section to get the IP address, or enter the Hostname directly in PuTTY.
Once you find the IP address, launch PuTTY, select Session, enter the IP address of the Raspberry Pi, and click Open.
Enter the username and password given at the time of flashing and click Enter.
Note: If you do not provide the username and password while flashing, then by default: Username: ubuntu Password: ubuntu
Switch to root mode and navigate to path /home/ubuntu/connectedhomeip/out/standalone to find the chip-tool. On the pre-built Matter Hub image, the chip-tool will be ready and working. Keep the PuTTY session open for the further steps.
If you are building the chip-tool from scratch, update the latest packages by running the following commands in the terminal:
$ sudo apt update $ sudo apt installInstall the required packages using the following commands:
$ sudo apt-get install git gcc g++ pkg-config libssl-dev libdbus-1-dev libglib2.0-dev libavahi-client-dev ninja-build python3-venv python3-dev python3-pip unzip libgirepository1.0-dev libcairo2-dev libreadline-devIf you see any popups between installs, you can select OK or Continue.
Build Environment#
Installing prerequisites on Raspberry Pi 4. Follow the instructions in the Project CHIP GitHub Site, in the section "Installing prerequisites on Raspberry Pi 4".
To build the environment, follow the steps in the Light and Switch Step-by-Step Example.
Bluetooth Setup#
Because Bluetooth LE (BLE) is used for commissioning on Matter, make sure BLE is up and running on Raspberry Pi. Raspberry Pi internally has some issues with BLE that may cause it to crash.
$ sudo systemctl status bluetooth.serviceTo stop BLE if it is already running:
$ sudo systemctl stop bluetooth.serviceTo restart the Bluetooth service, first enable it:
$ sudo systemctl enable bluetooth.serviceWhen you check the status of the Bluetooth service, it will be inactive because it has been enabled but not restarted:
$ sudo systemctl status bluetooth.serviceRestart the service:
$ sudo systemctl restart bluetooth.serviceNow the status of the service should be active and running:
$ sudo systemctl status bluetooth.service