Using Events and Timers with the Silicon Labs Matter Extension#
Event Handler#
The Matter event handler uses the FreeRTOS queue to transport a message from the producer to the consumer area. Events can be used to create asynchronous message processing or inter-task communication.
Depending on your sample app, instructions apply. See Application Customization Models.
Steps to make an event work:
Make sure the queue is initialized
Create an AppEventType for your application
Populate the Type and Handler variables
Post the message to the queue
Event definition enum#
AppEvent contains event types and event structures that are used for specific applications, if needed. Handler is used to store the callback for the event.
struct AppEvent
{
enum AppEventTypes
{
kEventType_Button = 0,
kEventType_Timer,
kEventType_Light,
kEventType_Install,
kEventType_Observer,
};
uint16_t Type;
union
{
struct
{
uint8_t Action;
} ButtonEvent;
struct
{
void * Context;
} TimerEvent;
struct
{
uint8_t Action;
int32_t Actor;
} LightEvent;
};
EventHandler Handler;
};Queue Posting#
When creating an event and pushing it to the event queue at minimum, Handler and Type must be defined in order for the event to work.
New Architecture#
Custom event posting and handlers are overridden in the CustomerAppTask file, not in autogen/AppTask.cpp.
void CreateObserverEvent(void)
{
AppEvent active_mode_event = {};
active_mode_event.Type = AppEvent::kEventType_Observer;
active_mode_event.Handler = SilabsSensors::SendSensorsValues;
AppInstance().PostEvent(&active_mode_event);
}Legacy Architecture#
Post events from src/AppTask.cpp:
void AppTask::CreateObserverEvent(void)
{
AppEvent active_mode_event = {};
active_mode_event.Type = AppEvent::kEventType_Observer;
active_mode_event.Handler = SilabsSensors::SendSensorsValues;
sAppTask.PostEvent(&active_mode_event);
}Callback#
Observer event callback
void SilabsSensors::SendSensorsValues(AppEvent * aEvent)
{
// Do something
}Dispatcher#
AppTaskMain is dispatching all the events from the event list.
New Architecture#
void AppTask::AppTaskMain(void * pvParameter)
{
AppEvent event;
QueueHandle_t sAppEventQueue = *(static_cast<QueueHandle_t *>(pvParameter));
CHIP_ERROR err = AppInstance().Init();
if (err != CHIP_NO_ERROR)
{
SILABS_LOG("AppTask.Init() failed");
appError(err);
}
#if !(defined(CHIP_CONFIG_ENABLE_ICD_SERVER) && CHIP_CONFIG_ENABLE_ICD_SERVER)
AppInstance().StartStatusLEDTimer();
#endif
AppInstance().RegisterObserver();
SILABS_LOG("App Task started");
while (true)
{
BaseType_t eventReceived = xQueueReceive(sAppEventQueue, &event, portMAX_DELAY);
while (eventReceived == pdTRUE)
{
AppInstance().DispatchEvent(&event);
eventReceived = xQueueReceive(sAppEventQueue, &event, 0);
}
}
}Legacy Architecture#
void AppTask::AppTaskMain(void * pvParameter)
{
AppEvent event;
QueueHandle_t sAppEventQueue = *(static_cast<QueueHandle_t *>(pvParameter));
CHIP_ERROR err = sAppTask.Init();
if (err != CHIP_NO_ERROR)
{
SILABS_LOG("AppTask.Init() failed");
appError(err);
}
#if !(defined(CHIP_CONFIG_ENABLE_ICD_SERVER) && CHIP_CONFIG_ENABLE_ICD_SERVER)
sAppTask.StartStatusLEDTimer();
#endif
sAppTask.RegisterObserver();
SILABS_LOG("App Task started");
while (true)
{
BaseType_t eventReceived = xQueueReceive(sAppEventQueue, &event, portMAX_DELAY);
while (eventReceived == pdTRUE)
{
sAppTask.DispatchEvent(&event);
eventReceived = xQueueReceive(sAppEventQueue, &event, 0);
}
}
}Matter Timer#
Start#
Initialize a one-shot timer to expire in 10 seconds and invoke TestCallback upon expiration.
System::Clock::Timeout Timeout = System::Clock::Seconds32(10);
chip::DeviceLayer::PlatformMgr().LockChipStack();
err = DeviceLayer::SystemLayer().StartTimer(Timeout, TestCallback, this);
chip::DeviceLayer::PlatformMgr().UnlockChipStack();Callback#
New Architecture#
Timer callback. Implement in src/CustomerAppTask.cpp.
void TestCallback(System::Layer * layer, void * aAppState)
{
// Do something
}Legacy Architecture#
Timer callback. Implement in src/AppTask.cpp.
void AppTask::TestCallback(System::Layer * layer, void * aAppState)
{
// Do something
}If you need a periodic timer, you can recall StartTimer() in the callback.