Edit

Matter + AWS Dual Stack Overview#

The dual-stack flavor of Matter + AWS is a Silicon Labs–specific configuration for 917 NCP (Network Co-Processor) designs. It enables Matter devices to connect locally to the Matter fabric over IPv6 through the EFR32 host and to AWS over IPv4 through the SiWx917 network wireless processor (NWP).

Note: Dual-stack here is not classic single-stack IPv4+IPv6 on one TCP/IP stack. It is a split-stack NCP architecture with separate network stacks on the host and the NWP.

When to Use the Dual-Stack Flavor#

Use the dual-stack flavor when all of the following apply:

  • Your design uses a 917 NCP board (EFR32 host + SiWx917 co-processor over SPI).

  • You need Matter + AWS (Direct Internet Connectivity) on that NCP platform.

  • Matter traffic must remain on IPv6 on the EFR32 host LwIP stack.

  • AWS MQTT/TLS traffic must run over IPv4 on the SiWx917 NWP offload stack.

For 917 SoC or standard 917 NCP builds that use a single host LwIP stack for both Matter and AWS, use the standard Matter + AWS build procedure instead.

Dual-Stack Architecture#

The following diagram shows how traffic is divided between the EFR32 host and the SiWx917 NWP.

Matter + AWS dual-stack architectureMatter + AWS dual-stack architecture

Traffic path

Processor

Network stack

Protocol

Matter fabric, mDNS, CASE

EFR32 host

Host LwIP

IPv6

Wi-Fi radio association

SiWx917 NWP

Offload stack

—

AWS MQTT/TLS

SiWx917 NWP

sl_si91x_socket (NWP offload)

IPv4

The EFR32 host and SiWx917 NWP communicate over the SPI NCP interface. The Matter Dual Stack component (matter_dual_stack) replaces the standard Matter LwIP component (matter_lwip) and defines the build macro SL_MATTER_ENABLE_DUAL_STACK=1.

Flavor Comparison#

Setting

917 SoC Matter + AWS

Standard 917 NCP Matter + AWS

917 NCP Dual-Stack Matter + AWS

Network provider

matter_lwip

matter_lwip

matter_dual_stack

AWS transport

matter_aws_transport_lwip

matter_aws_transport_lwip

matter_aws_transport_nwp

MQTT/TLS path

Host LwIP altcp

Host LwIP altcp

NWP sl_si91x_socket

Matter protocol

IPv6 (host LwIP)

IPv6 (host LwIP)

IPv6 (host LwIP)

AWS/cloud protocol

IPv4 (host LwIP)

IPv4 (host LwIP)

IPv4 (NWP offload)

BLE for commissioning

SoC BLE

matter_wifi_ble (917)

matter_ble (EFR32 host)

IPv6 project define

via matter_lwip

via matter_lwip

SLI_SI91X_ENABLE_IPV6=1

Dual-stack build macro

—

—

SL_MATTER_ENABLE_DUAL_STACK=1

The AWS transport components matter_aws_transport_lwip and matter_aws_transport_nwp are mutually exclusive. Install exactly one transport with the Matter AWS component.

Component and Macro Checklist#

When building a dual-stack Matter + AWS application, verify the following:

Item

Dual-stack value

Network stack provider

matter_dual_stack (not matter_lwip)

AWS transport

matter_aws_transport_nwp (not matter_aws_transport_lwip)

BLE component

matter_ble (not matter_wifi_ble)

Matter Wi-Fi IPv4 setting

Enable CHIP_DEVICE_CONFIG_ENABLE_IPV4

Project define

SLI_SI91X_ENABLE_IPV6=1

Build macro (automatic)

SL_MATTER_ENABLE_DUAL_STACK=1 (set by matter_dual_stack)

AWS dependencies

mbedtls_x509_use_aws, mbedtls_x509_create_aws, mbedtls_entropy_default_aws

917 NCP TLS

psa_crypto_tls12_prf (TLS 1.2 PRF)

Supported Hardware and Software#

Hardware#

Dual-stack Matter + AWS is supported on 917 NCP Radio boards only(BRD4346A):

  • BRD4186C

  • BRD4187C

  • BRD4120A

Standard Matter + AWS on 917 SoC and standard 917 NCP boards is documented separately. See Prerequisites on the Matter + AWS index page.

Software#

  • Matter Extension 2.9.1 or later

  • WiseConnect SDK 4.1.1 or later

  • Correct SiWx917 NCP connectivity firmware supporting dual network stack mode

Reference Example#

The Matter Extension provides a reference door lock application for dual-stack builds:

  • Project: matter_wifi_917_ncp_lock_app_dual_stack_freertos

  • Description: Matter over Wi-Fi door lock with BLE on the EFR32 host (IPv6 on EFR32, IPv4 on SiWx917)

This is currently the only Matter example project configured for the dual-stack flavor.

Limitations#

  • 917 NCP only — not supported on 917 SoC or standard single-stack 917 NCP AWS builds.

  • Single reference app — only the lock app example is provided for dual-stack today.

  • Transport exclusivity — do not install both matter_aws_transport_lwip and matter_aws_transport_nwp in the same project.

Next Steps#