Matter + AWS Dual Stack Overview#
The dual-stack flavor of Matter + AWS is a Silicon Labs–specific configuration for 917 NCP (Network Co-Processor) designs. It enables Matter devices to connect locally to the Matter fabric over IPv6 through the EFR32 host and to AWS over IPv4 through the SiWx917 network wireless processor (NWP).
Note: Dual-stack here is not classic single-stack IPv4+IPv6 on one TCP/IP stack. It is a split-stack NCP architecture with separate network stacks on the host and the NWP.
When to Use the Dual-Stack Flavor#
Use the dual-stack flavor when all of the following apply:
Your design uses a 917 NCP board (EFR32 host + SiWx917 co-processor over SPI).
You need Matter + AWS (Direct Internet Connectivity) on that NCP platform.
Matter traffic must remain on IPv6 on the EFR32 host LwIP stack.
AWS MQTT/TLS traffic must run over IPv4 on the SiWx917 NWP offload stack.
For 917 SoC or standard 917 NCP builds that use a single host LwIP stack for both Matter and AWS, use the standard Matter + AWS build procedure instead.
Dual-Stack Architecture#
The following diagram shows how traffic is divided between the EFR32 host and the SiWx917 NWP.


Traffic path | Processor | Network stack | Protocol |
|---|---|---|---|
Matter fabric, mDNS, CASE | EFR32 host | Host LwIP | IPv6 |
Wi-Fi radio association | SiWx917 NWP | Offload stack | — |
AWS MQTT/TLS | SiWx917 NWP |
| IPv4 |
The EFR32 host and SiWx917 NWP communicate over the SPI NCP interface. The Matter Dual Stack component (matter_dual_stack) replaces the standard Matter LwIP component (matter_lwip) and defines the build macro SL_MATTER_ENABLE_DUAL_STACK=1.
Flavor Comparison#
Setting | 917 SoC Matter + AWS | Standard 917 NCP Matter + AWS | 917 NCP Dual-Stack Matter + AWS |
|---|---|---|---|
Network provider |
|
|
|
AWS transport |
|
|
|
MQTT/TLS path | Host LwIP altcp | Host LwIP altcp | NWP |
Matter protocol | IPv6 (host LwIP) | IPv6 (host LwIP) | IPv6 (host LwIP) |
AWS/cloud protocol | IPv4 (host LwIP) | IPv4 (host LwIP) | IPv4 (NWP offload) |
BLE for commissioning | SoC BLE |
|
|
IPv6 project define | via | via |
|
Dual-stack build macro | — | — |
|
The AWS transport components matter_aws_transport_lwip and matter_aws_transport_nwp are mutually exclusive. Install exactly one transport with the Matter AWS component.
Component and Macro Checklist#
When building a dual-stack Matter + AWS application, verify the following:
Item | Dual-stack value |
|---|---|
Network stack provider |
|
AWS transport |
|
BLE component |
|
Matter Wi-Fi IPv4 setting | Enable |
Project define |
|
Build macro (automatic) |
|
AWS dependencies |
|
917 NCP TLS |
|
Supported Hardware and Software#
Hardware#
Dual-stack Matter + AWS is supported on 917 NCP Radio boards only(BRD4346A):
BRD4186C
BRD4187C
BRD4120A
Standard Matter + AWS on 917 SoC and standard 917 NCP boards is documented separately. See Prerequisites on the Matter + AWS index page.
Software#
Matter Extension 2.9.2 or later
WiseConnect SDK 4.1.2 or later
Correct SiWx917 NCP connectivity firmware supporting dual network stack mode
Reference Example#
The Matter Extension provides a reference door lock application for dual-stack builds:
Project:
matter_wifi_917_ncp_lock_app_dual_stack_freertosDescription: Matter over Wi-Fi door lock with BLE on the EFR32 host (IPv6 on EFR32, IPv4 on SiWx917)
This is currently the only Matter example project configured for the dual-stack flavor.
Limitations#
917 NCP only — not supported on 917 SoC or standard single-stack 917 NCP AWS builds.
Single reference app — only the lock app example is provided for dual-stack today.
Transport exclusivity — do not install both
matter_aws_transport_lwipandmatter_aws_transport_nwpin the same project.
Next Steps#
Build Procedure for Matter + AWS Dual Stack: For component installation and project configuration.
Build Procedure for Matter + AWS (standard flavor): For 917 SoC and standard 917 NCP.
Matter + AWS index: For AWS cloud setup, end-to-end testing, and shared configuration.