Matter Hardware Requirements#
To run Matter over Thread or over Wi-Fi requires some Silicon Labs hardware in order to run demos and do development. Following are the hardware requirements for both Thread and Wi-Fi use cases broken down by platform and transport protocol.
The following sections describe the hardware that may be used for Matter+OpenThread (Matter Hub and Accessory Device) and for Matter+Wi-Fi (Accessory Device). The EFR32MG24/MG26 is the preferred starting point for Matter MCUs (including the Matter Hub RCP and both Accessory Devices). It provides Secure Vault and can use the internal flash of the device to store an upgrade image. The EFR32MG24/MG26 is recommended for running the Matter over Thread and Matter over Wi-Fi Quick-Start guides.
Matter Over Thread "Matter Hub" Requirements#
If you are running Matter over Thread and do not have a platform on which to run the Open Thread Border Router and chip-tool, Silicon Labs recommends that you run them on a Raspberry Pi. To do so you will need:
Raspberry Pi
Raspberry Pi 4 with an SD card with storage >= 64 GB
The Raspberry Pi 4 is used to run the Open Thread Border Router and the chip-tool. In this documentation the combination of this software on the Raspberry Pi is also called the 'Matter Hub' A software image for the Raspberry Pi is provided on the Matter Artifacts page.
Radio Co-Processor (RCP)
The Matter Hub needs a 15.4 RCP in order to create and interact with the Thread network. The RCP can be any Silicon Labs development board that is capable of running the OpenThread RCP firmware. The RCP radio board is connected to the Raspberry Pi via USB.
Over 60 Silicon Labs boards support running the RCP firmware. To build an image for a board that is not listed here, download and build your image in Simplicity Studio. Pre-built OpenThread RCP firmware images are provided for the following boards on the Matter Artifacts page:
Note: The EFR32MG24/MG26 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
MGM24 boards:
BRD4316A / SLWSTK6006A / Wireless Start Kit / 2.4GHz@10dBm - xGM240-RB4316A
BRD4317A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4317A
BRD4318A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4318A
BRD4319A (Rev A00 only) / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm
BRD2704A / Sparkfun Thing Plus MGM240P
BRD4337A / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xGM240-RB4337A
MG26 boards:
BRD4116A / 2.4GHz@10dBm
BRD4117A / 2.4GHz@20dBm
BRD4118A / 2.4GHz@20dBm
BRD4120A
BRD4121A
BRD2608A
BRD2709A
MGM26 boards:
BRD4350A
BRD4351A
Matter Over Thread Accessory Device Requirements#
The Matter Accessory Device (MAD) is the actual device that the Matter application firmware (such as the Matter Light or Matter Switch) runs on. Several different platforms for the MAD are supported. Pre-built binary images for the MADs are provided on the Matter Artifacts page. Silicon Labs supports development of MADs for Matter over Thread on the following platforms:
Note: The EFR32MG24/MG26 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
MG24 boards
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
BRD2703A / MG24 Explorer Kit
BRD2601B / MG24 Explorer Kit
MGM24 boards:
BRD4316A / SLWSTK6006A / Wireless Start Kit / 2.4GHz@10dBm - xGM240-RB4316A
BRD4317A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4317A
BRD4318A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4318A
BRD4319A (Rev A00 only) / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm
BRD2704A / Sparkfun Thing Plus MGM240P
BRD4337A / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xGM240-RB4337A
MG26 boards
BRD4116A / 2.4GHz@10dBm
BRD4117A / 2.4GHz@20dBm
BRD4118A / 2.4GHz@20dBm
BRD4120A
BRD4121A
BRD2608A
BRD2709A
MGM26 boards:
BRD4350A
BRD4351A
MGM301 boards:
BRD2719A
BRD4407A
BRD4408A
Matter Over Wi-Fi Accessory Device Requirements#
Matter Over Wi-Fi Accessory Device Requirements for NCP Mode#
The Silicon Labs Matter over Wi-Fi NCP mode demo and development requires two boards: the Silicon Labs EFR32 Radio board to run the Matter code and either the SiWx917 or WF200 to run the Wi-Fi protocol stack. Pre-built images for the EFR32, and also for SiWx917 connectivity firmware, are provided on the Matter Artifacts page.
Notes:
The EFR32MG24/MG26 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
The WF200 connectivity firmware image is included in the EFR32MG24 images on the Matter Artifacts page for running with the WF200 in NCP mode. The Matter application downloads the connectivity firmware onto the WF200 on first-time startup.
The following boards are supported for the Matter over Wi-Fi demos and development:
MG24 boards
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm
MG24 with WSTK : xG24-PK6009A
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm
MG24 with WSTK : xG24-PK6010A
Wi-Fi NCP Dev Kits & boards
SiWx917 NCP
SiWx917 NCP Mode / Wi-Fi Expansion Board / 2.4GHz
BRD8045A (B0 Expansion v2.0)
WF200
WF200 / Single Band Wi-Fi Expansion Board / 2.4GHz
WF200 / Single Band Wi-Fi Expansion Board / 2.4GHz
Matter over Wi-Fi Accessory Device Requirements for SoC Mode#
The Silicon Labs Matter over Wi-Fi demo and development for SoC mode requires the SiWx917 SoC board that supports Matter over Wi-Fi in a single-chip package. The integrated MCU is dedicated for peripheral and application-related processing (Matter), while the ThreadArch® runs the wireless and networking protocol stacks.
Pre-built images for the SiWx917 connectivity firmware are available as per the instructions on the Matter Artifacts page. The following boards are supported for the Matter over Wi-Fi demos and development:
Wi-Fi SoC boards
BRD4338A / SiWx917 Wi-Fi 6 and Bluetooth LE 8 MB Flash SoC Pro Kit - SiWx917-PK6031A
BRD2605A / SiWx917 Wi-Fi 6 and Bluetooth LE Dev Kit - SiWx917-DK2605A
BRD4342A / SiWx917 Wi-Fi 6 and Bluetooth LE 8 MB Flash + 8 MB ext PSRAM Radio Board with an internal RF switch - SiWx91x-RB4342A
Note: Refer to SiWx917 SoC for more details.
Additional Matter Over Wi-Fi Hardware Requirements#
In addition to your Matter over Wi-Fi Accessory Device, you need the following for both running the demo and for development:
Windows/Linux/MacOS computer with a USB port
USB cable for connecting WSTK Board to Computer
Raspberry Pi with a >32 GB SD Card
Access point with Internet access
microSD card (>=32GB) (if using Raspberry Pi)
[Optional] Android Mobile phone (If using the chip-tool on Android)