Codex#

To install the Silicon Labs MCP Server in Codex, complete the following steps:

Install MCP: codex mcp add silicon-labs-docs -- https://silabs.mcp.kapa.ai/.

The ~/.codex/config.toml file can also be manually configured:

~/.codex/config.toml

[mcp_servers.silicon-labs-docs]
command = "https://silabs.mcp.kapa.ai"

Note: As of version 0.112, a bug affecting internal projects can cause authentication to fail. As a workaround, add the following parameter to the authorization URL generated by Codex: &resource=https%3A%2F%2Fsilabs.mcp.kapa.ai%2F