Gecko Bootloader API Reference
To use the application interface in your application, include the api/btl_interface.h header in your application, and add the following files to the build:
- api/btl_interface.c
 - api/btl_interface_storage.c See the Application Interface documentation for more information.
 
Bootloader Components
The bootloader itself consists of multiple parts:
Core
The bootloader core contains the main function of both bootloader stages. It also contains functionality to write to the internal main flash, to perform a bootloader upgrade, and to reset into the application flagging applicable reset reasons. See the core documentation for more information.
Driver
Different bootloading applications require different hardware drivers for use by the other components of the bootloader. See the driver documentation for more information.
Plugin
All parts of the bootloader that are either optional or swappable for different implementations are implemented as plugins. Each plugin has a generic header file, and one or more implementations. The current release contains plugins for functionality like UART and SPI communication protocols, SPI flash storage, internal flash storage, and different cryptographic operations. For more information about the different plugins, see the plugin documentation.