Reset
Description
Methods to reset from the bootloader to the app.
Functions |
|
| void | reset_resetWithReason (uint16_t resetReason) |
| void | reset_setResetReason (uint16_t resetReason) |
| void | reset_enableResetCounter (void) |
| void | reset_disableResetCounter (void) |
| bool | reset_resetCounterEnabled (void) |
| void | reset_incrementResetCounter (void) |
| uint8_t | reset_getResetCounter (void) |
| uint16_t | reset_getResetReason (void) |
| void | reset_invalidateResetReason (void) |
| uint16_t | reset_classifyReset (void) |
Function Documentation
| void reset_resetWithReason | ( | uint16_t |
resetReason
|
) |
Reset from the bootloader with a reset cause.
- Note
- This function does not return.
- Parameters
-
resetReasonA reset reason as defined in the bootloader interface
| void reset_setResetReason | ( | uint16_t |
resetReason
|
) |
Set a reset reason.
- Parameters
-
resetReasonA reset reason as defined in the bootloader interface
| void reset_enableResetCounter | ( | void |
|
) |
Use the lower 4 bits of the reset cause signature to store a reset counter able to count up to 15 before wrapping around. The value of the counter will be preserved across resets.
| void reset_disableResetCounter | ( | void |
|
) |
Clear and disable the reset counter.
| bool reset_resetCounterEnabled | ( | void |
|
) |
Check if the reset counter is enabled.
- Returns
- True if reset counter is enabled, else false.
| void reset_incrementResetCounter | ( | void |
|
) |
Increment the reset counter by one.
Wraps around to 0 if the current counter value is equal to 15.
| uint8_t reset_getResetCounter | ( | void |
|
) |
Get the reset counter value.
- Note
- The reset counter has to be enabled for this value to be valid.
- Returns
- The reset counter value
| uint16_t reset_getResetReason | ( | void |
|
) |
Get the reset reason without verifying it.
- Returns
- The reset reason
| void reset_invalidateResetReason | ( | void |
|
) |
Invalidate the reset reason.
- Note
- This will also disable the reset counter if it is in use.
| uint16_t reset_classifyReset | ( | void |
|
) |
Classify reset and get the reset reason.
- Returns
- Reset cause or BOOTLOADER_RESET_REASON_UNKNOWN