SHA_256Plugin > Security
Description
SHA-256 digest functionality for the bootloader.
Data Structures |
|
| union | Sha256Context |
|
Context type for SHA algorithm.
|
|
Macros |
|
| #define | BTL_SECURITY_SHA256_DIGEST_LENGTH 32 |
|
Number of bytes in a SHA-256 digest.
|
|
Typedefs |
|
| typedef union Sha256Context | Sha256Context_t |
|
Context type for SHA algorithm.
|
|
Functions |
|
| void | btl_initSha256 (void *ctx) |
| void | btl_updateSha256 (void *ctx, const void *data, size_t length) |
| void | btl_finalizeSha256 (void *ctx) |
| int32_t | btl_verifySha256 (void *ctx, const void *sha256) |
Function Documentation
| void btl_initSha256 | ( | void * |
ctx
|
) |
Initialize SHA256 context variable
- Parameters
-
ctxPointer to the SHA256 context variable to be initialized
Wipes out the SHA256 context variable and sets it up for re-use.
| void btl_updateSha256 | ( | void * |
ctx,
|
| const void * |
data,
|
||
| size_t |
length
|
||
| ) |
Run data through the SHA256 hashing function
- Parameters
-
ctxPointer to the SHA256 context variable dataPointer to array of binary data to add to the SHA256 calculation in progress lengthLength of the byte array with data.
| void btl_finalizeSha256 | ( | void * |
ctx
|
) |
Finalize SHA256 calculation
- Parameters
-
ctxPointer to the SHA256 context variable to be initialized
Finalizes the running SHA256 calculation. After finalization, the SHA value in the context variable will be valid, and no more data can be added.
| int32_t btl_verifySha256 | ( | void * |
ctx,
|
| const void * |
sha256
|
||
| ) |
Compare SHA256 from context variable to a known value
- Parameters
-
ctxPointer to the SHA256 context variable to be initialized sha256Byte array containing sha256 value to compare to
- Returns
- BOOTLOADER_OK if both hash values are equal, else error code from BOOTLOADER_ERROR_SECURITY_BASE range.
Convenience function to compare a known SHA256 hash against the result of a calculation.