CommunicationComponents
Description
Host communication interface.
The Communication component provides an interface for implementing communication with a host device, such as a computer or a microcontroller.
Communication Protocol Implementations
Several components implement the communication interface, using different transports and protocols.
Bluetooth Apploader OTA DFU
BGAPI UART DFU
EZSP-SPI
ezsp-spi-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks.
UART XMODEM
serial-uart-bootloader
that was previously released with the EmberZnet and SL-Thread wireless stacks.
Modules |
|
| Utils | |
Function Documentation
| void bootloader_apploader_communication_init | ( | void |
|
) |
Initialize hardware for the BLE Apploader OTA DFU Bootloader communication.
| int32_t bootloader_apploader_communication_start | ( | void |
|
) |
Initialize communication between the BLE Apploader OTA DFU bootloader and external host.
- Returns
- Error code indicating success or failure.
| int32_t bootloader_apploader_communication_main | ( | ImageProperties_t * |
imageProps,
|
| ParserContext_t * |
parserContext,
|
||
| DecryptContext_t * |
decryptContext,
|
||
| AuthContext_t * |
authContext,
|
||
| const BootloaderParserCallbacks_t * |
parseCb
|
||
| ) |
Communication main for the BLE Apploader OTA DFU bootloader.
- Parameters
-
imagePropsThe image file processed parserContextImage parser context decryptContextImage decryption context authContextImage authentication context parseCbBootloader parser callbacks
- Returns
- Error code indicating success or failure.
| void bootloader_bgapi_communication_init | ( | void |
|
) |
Initialize hardware for the BGAPI UART DFU Bootloader communication.
| int32_t bootloader_bgapi_communication_start | ( | void |
|
) |
Initialize communication between the BGAPI UART DFU bootloader and external host.
- Returns
- Error code indicating success or failure.
| int32_t bootloader_bgapi_communication_main | ( | ImageProperties_t * |
imageProps,
|
| ParserContext_t * |
parserContext,
|
||
| const BootloaderParserCallbacks_t * |
parseCb
|
||
| ) |
Communication main for the BGAPI UART DFU bootloader.
- Parameters
-
imagePropsThe image file processed parserContextImage parser context parseCbBootloader parser callbacks
- Returns
- Error code indicating success or failure.
| void communication_init | ( | void |
|
) |
Initialize hardware for the communication component.
| int32_t communication_start | ( | void |
|
) |
Initialize communication between the bootloader and external host. For example, indicate that all is well to the external host.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OKon success BOOTLOADER_ERROR_COMMUNICATION_STARTon failure
| int32_t communication_main | ( | void |
|
) |
Not supposed to return until either the host signals the end of the current session or a new image has been flashed and verified.
- Returns
- Error code indicating success or failure
- Return values
-
BOOTLOADER_OKwhen a new image was flashed BOOTLOADER_ERROR_COMMUNICATION_ERRORon communication error BOOTLOADER_ERROR_COMMUNICATION_DONEwhen no image was received BOOTLOADER_ERROR_COMMUNICATION_IMAGE_ERRORwhen received image is invalid
| void communication_shutdown | ( | void |
|
) |
Stop communication between the bootloader and external host.
| void bootloader_ezsp_communication_init | ( | void |
|
) |
Initialize hardware for the EZSP SPI Bootloader communication.
| int32_t bootloader_ezsp_communication_start | ( | void |
|
) |
Initialize communication between the EZSP SPI bootloader and external host.
- Returns
- Error code indicating success or failure.
| int32_t bootloader_ezsp_communication_main | ( | ImageProperties_t * |
imageProps,
|
| ParserContext_t * |
parserContext,
|
||
| const BootloaderParserCallbacks_t * |
parseCb
|
||
| ) |
Communication main for the EZSP SPI bootloader.
- Parameters
-
imagePropsThe image file processed parserContextImage parser context parseCbBootloader parser callbacks
- Returns
- Error code indicating success or failure.
| void bootloader_ezsp_communication_shutdown | ( | void |
|
) |
Stop communication between the bootloader and external host.
| void bootloader_xmodem_communication_init | ( | void |
|
) |
Initialize hardware for the UART XMODEM Bootloader communication.
| int32_t bootloader_xmodem_communication_start | ( | void |
|
) |
Initialize communication between the UART XMODEM bootloader and external host.
- Returns
- Error code indicating success or failure.
| int32_t bootloader_xmodem_communication_main | ( | ImageProperties_t * |
imageProps,
|
| const BootloaderParserCallbacks_t * |
parseCb
|
||
| ) |
Communication main for the UART XMODEM bootloader.
- Parameters
-
imagePropsThe image file processed parseCbBootloader parser callbacks
- Returns
- Error code indicating success or failure.