Bootloader Core
Description
Core bootloader functionality.
Core functionality for the Silicon Labs Bootloader.
Modules |
|
| Bootload | |
|
Methods to verify and bootload application images.
|
|
| Flash | |
|
Interface to internal flash.
|
|
| Reset | |
|
Methods to reset from the bootloader to the app.
|
|
| TrustZone | |
|
TrustZone utilities.
|
|
| Upgrade | |
|
Methods to verify and upgrade the main bootloader.
|
|
Macros |
|
| #define | BOOTLOADER_ENFORCE_SIGNED_UPGRADE |
|
The bootloader will enforce signed upgrade images.
|
|
| #define | BOOTLOADER_ENFORCE_ENCRYPTED_UGPRADE |
|
The bootloader will enforce encrypted upgrade images.
|
|
| #define | BOOTLOADER_ENFORCE_SECURE_BOOT |
|
The bootloader will enforce signed applications.
|
|
| #define | BOOTLOADER_SUPPORT_STORAGE |
|
The bootloader supports the storage interface (application bootloader)
|
|
| #define | BOOTLOADER_SUPPORT_COMMUNICATION |
|
The bootloader supports the communication interface (standalone bootloader)
|
|
| #define | BTL_APP_SPACE_SIZE |
|
Size of the area set aside for the application.
|
|
Functions |
|
| int32_t | btl_init (void) |
| int32_t | btl_deinit (void) |
Macro Definition Documentation
| #define BTL_APP_SPACE_SIZE |
Size of the area set aside for the application.
During firmware upgrade, the bootloader will ensure that the new application image is within the boundaries set by the start of the application and the start + the value of this define. If using an NVM system, the size of this define can be reduced to protect the NVM system from being overwritten by an attempted application upgrade using a too large application image.
Definition at line
51
of file
btl_capabilities.h
.
Function Documentation
| int32_t btl_init | ( | void |
|
) |
Initialize bootloader.
- Returns
- Error code. BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_INIT_BASE range.
| int32_t btl_deinit | ( | void |
|
) |
Deinitialize bootloader.
- Returns
- Error code. BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_INIT_BASE range.