Information about the current bootloader.
Public Attributes#
uint16_t
Version, either of the bootloader for standalone bootloaders or of the storage info struct for application bootloaders.
The type of bootloader.
uint32_t
Version number of the bootloader.
uint32_t
Capability mask for the bootloader.
Public Attribute Documentation#
version#
uint16_t BootloaderInformation_t::version
Version, either of the bootloader for standalone bootloaders or of the storage info struct for application bootloaders.
Definition at line
122
of file platform/bootloader/api/ember_btl_interface.h
type#
BootloaderType_t BootloaderInformation_t::type
The type of bootloader.
Definition at line
113
of file platform/bootloader/api/btl_interface.h
version#
uint32_t BootloaderInformation_t::version
Version number of the bootloader.
Definition at line
115
of file platform/bootloader/api/btl_interface.h
capabilities#
uint32_t BootloaderInformation_t::capabilities
Capability mask for the bootloader.
Definition at line
117
of file platform/bootloader/api/btl_interface.h