EZSP GPIO#
Enter bootloader based on EZSP GPIO state.
The EZSP communication protocol over SPI can be used together with this component.
By enabling the EZSP GPIO component, the firmware upgrade mode can be entered by activating the nWake pin.
Functions#
bool
Enter the bootlader if the GPIO pin is active.
Function Documentation#
ezsp_gpio_enterBootloader#
bool ezsp_gpio_enterBootloader (void )
Enter the bootlader if the GPIO pin is active.
Parameters
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
Returns
True if the bootloader should be entered
Definition at line
38
of file platform/bootloader/gpio/ezsp-gpio-activation/btl_ezsp_gpio_activation.h