GBL tag parsing info struct. Contains information about the GBL tag order, etc.

Public Attributes#

uint32_t

Tag ID.

The parser state associated with the tag.

uint8_t

Encodes correct order of occurrence in GBL.

uint8_t

Reserved.

uint16_t

Flags defining parser behavior.

Public Attribute Documentation#

tagId#

uint32_t GblTagParsingInfo_t::tagId

Tag ID.


Definition at line 145 of file platform/bootloader/parser/gbl/btl_gbl_parser.h

parserState#

GblParserState_t GblTagParsingInfo_t::parserState

The parser state associated with the tag.


Definition at line 146 of file platform/bootloader/parser/gbl/btl_gbl_parser.h

tagOrder#

uint8_t GblTagParsingInfo_t::tagOrder

Encodes correct order of occurrence in GBL.


Definition at line 147 of file platform/bootloader/parser/gbl/btl_gbl_parser.h

reserved#

uint8_t GblTagParsingInfo_t::reserved

Reserved.


Definition at line 148 of file platform/bootloader/parser/gbl/btl_gbl_parser.h

flags#

uint16_t GblTagParsingInfo_t::flags

Flags defining parser behavior.


Definition at line 149 of file platform/bootloader/parser/gbl/btl_gbl_parser.h